IMX8XQP UUU下载imx-p9.0.0_2.1.0-auto-ga失败([HID(W):LIBUSB_ERROR_IO)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8XQP UUU下载imx-p9.0.0_2.1.0-auto-ga失败([HID(W):LIBUSB_ERROR_IO)

869件の閲覧回数
jianhua_zhuang
Contributor I

编译imx-p9.0.0_2.1.0-auto-ga基线的镜像;使用uuu命令下载到eMMC失败。

E:\IMX8QXP_image\mek>uuu_imx_android_flash.bat -f imx8qxp -e -a
This script is validated with uuu 1.2.91 version, please align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash spl-imx8qxp.bin to the partition of bootloader0
generate lines to flash bootloader-imx8qxp.img to the partition of bootloader_a
generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.43-0-ga9c099a

Success 0 Failure 1


2:4 1/ 1 [HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f u-boot-imx8qxp-mek-uuu.imx.link

 

0 件の賞賛
返信
0 返答(返信)