IMX8QXP

cancel
Showing results for 
Search instead for 
Did you mean: 

IMX8QXP

682 Views
shalanyang
Contributor II

how many uarts in imxqxp(imx8qxp support) ? Include scufw+seco+atf(tee)+m4+uboot,and they have some relationship between them, who could tell me ?

0 Kudos
1 Reply

514 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

 

  

  According to Figure 1 (i.MX 8QuadXPlus/8DualXPlus System Block Diagram) of the i.MX 8X Datasheet(s),

there are the following UARTs: User CM4 UART, SCU CM4 UART, and 4 shared UARTs.

 

 Section 5.1 (Overview) of the i.MX 8DualXPlus/8QuadXPlus Reference Manual describes boot process.

 

  The i.MX 8QuadXPlus MEK Board has two independent UART Ports (UART0, M40_UART0) for debugging:

UART0_TX & UART0_RX are used to output serial debugging information for A35-core.

M40_UART0_TX & M40_UART0_RX are used to output serial debugging information for M4-core.

 

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos