IMX8QXP uses Q10.0.0_2.2.0_AUTO_SOURCE and requires NVP6324 driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QXP uses Q10.0.0_2.2.0_AUTO_SOURCE and requires NVP6324 driver

651件の閲覧回数
relax-wu
Contributor IV

The current project uses NVP6324, is there a corresponding driver patch?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

640件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi relax-wu

 

please refer to below patch:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Nvp6324-driver-for-imx8qm/ta-p/1114616

 

Best regards
igor

0 件の賞賛
返信

630件の閲覧回数
relax-wu
Contributor IV

Hi

If the driver migration is successful and the hardware path is normal, is it tested through the camera application that comes with the system?

0 件の賞賛
返信