【IMX8QXP,PMIC】Where the PMIC control logic in code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

【IMX8QXP,PMIC】Where the PMIC control logic in code?

Jump to solution
1,592 Views
jianwei_lan
Contributor III

Dear friend

My platform is IMX8QXP MEK. Linux 5.4.70.

I want to do some change on PMIC control, can you provide information about where I can do some modification in code? And also, other info related are welcome.

 

----

BR 

0 Kudos
Reply
1 Solution
1,590 Views
Kazuma_Sasaki
Senior Contributor I
0 Kudos
Reply
1 Reply
1,591 Views
Kazuma_Sasaki
Senior Contributor I

Hi,

PMIC control by SCU. so, You need investigating the SCFW porting kit.

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=L5.4.70_2.3.0_SCFWKIT-1.7.0&appType=file...

Also, following information will be useful.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

Best Regards,

Kazuma Sasaki.

0 Kudos
Reply