IMX8QM mSATA use internal clk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM mSATA use internal clk

823 Views
smarter
Contributor II

our designed board use msata only  ,so there is not external clk source ,so we set ext_osc =0 . boot log occur 

[ 1.440584] iommu: Adding device 5f020000.sata to group 0
[ 1.449801] ahci-imx 5f020000.sata: internal pll is used.
[ 1.455363] ahci-imx 5f020000.sata: TX PLL of the PHY is not locked
[ 1.461644] ahci-imx 5f020000.sata: failed to reset phy: -19

how can i resolve this issue? thank you!

0 Kudos
Reply
1 Reply

765 Views
igorpadykov
NXP Employee
NXP Employee

Hi bin

sata currently is not supported as described on p.21

i.MX 8QuadMax Automotive and Infotainment Applications Processors

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply