IMX8QM: imx-mkimage failed to build the linux image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM: imx-mkimage failed to build the linux image

1,599 Views
vinothkumars
Senior Contributor IV

Hi NXP Team,

 

I unable to build the kernel with m4 I got the following error, How to resolve this error (how to generate the u-boot-spl.bin)

 

$ make SOC=iMX8QM flash_linux_m4
include misc.mak
include m4.mak
include android.mak
include test.mak
include autobuild.mak
include alias.mak
make[1]: *** No rule to make target 'u-boot-spl.bin', needed by 'flash_linux_m4'. Stop.
make: *** [Makefile:23: flash_linux_m4] Error 2

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
2 Replies

1,565 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version of BSP are you using?

0 Kudos
Reply

1,564 Views
vinothkumars
Senior Contributor IV

Thank you @Rita_Wang  for the reply,

 

I am using LF5.10.35_2.0.0

U-Boot -  v2021.04

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply