Hi, expert,
I am looking at the imx8qm DTS file in linux-imx kernel git branch imx_4.14.98_2.0.0_ga. The IMX8qm SoC has two I2C buses for each ldb brdige. But in the file: arch/arm64/boot/dts/freescale/fsl-imx8qm-device.dtsi, only one I2C of each ldb used. Strange that the i2c1_lvds0 is connected to i2c0_clk (IMX8QM_LVDS0_I2C0_CLK)
i2c1_lvds0: i2c@56247000 { <-========================I2C1
compatible = "fsl,imx8qm-lpi2c";
reg = <0x0 0x56247000 0x0 0x1000>;
interrupts = <9 IRQ_TYPE_LEVEL_HIGH>;
interrupt-parent = <&irqsteer_lvds0>;
clocks = <&clk IMX8QM_LVDS0_I2C0_CLK>, <-----------I2C0 ??
<&clk IMX8QM_LVDS0_I2C0_IPG_CLK>; <----i2c0
clock-names = "per", "ipg";
assigned-clocks = <&clk IMX8QM_LVDS0_I2C0_CLK>;
assigned-clock-rates = <24000000>;
power-domains = <&pd_lvds0_i2c0>;
status = "disabled";
};
i2c1_lvds1: i2c@57247000 { <============================= i2C1
compatible = "fsl,imx8qm-lpi2c";
reg = <0x0 0x57247000 0x0 0x1000>;
interrupts = <9 IRQ_TYPE_LEVEL_HIGH>;
interrupt-parent = <&irqsteer_lvds1>;
clocks = <&clk IMX8QM_LVDS1_I2C0_CLK>, <--- I2C0
<&clk IMX8QM_LVDS1_I2C0_IPG_CLK>; <-- I2C0
clock-names = "per", "ipg";
assigned-clocks = <&clk IMX8QM_LVDS1_I2C0_CLK>;
assigned-clock-rates = <24000000>;
power-domains = <&pd_lvds1_i2c0>;
status = "disabled";
};
I have few questions about this:
1. Why the clock signals of i2c are cross connection ? clocks of i2c0 are connected to i2c1 master ??
2. If we change the cross connection, says connect clocks of i2c0 to i2c0 module, is there any trouble ? (any bugs in SCU firmware or hardware ??);
3. Can the two channels of each ldb bridge display different picture frames independently ?
4. If we want to set different brightness for the two panels'backlight connect to the two channels of the same ldb, how can we do that since there is only one PWM region (lvds0_pwm: pwm@56244000 for lvds0, lvds1_pwm: pwm@57244000 for lvds1) ?
5. In the i2c1_lvdsX node, it says that i2c use interrrupt 9 of irq_steer:
interrupts = <9 IRQ_TYPE_LEVEL_HIGH>;
If we want to enable i2c0_lvdsX, which interrupt number should we use ?
Best Regards,
-minskey
Hi,
minskey.guo@outlook.com were you able to use the I2C on LVDS ?
I am facing an issue where we use both I2C on the LVDS block but only I2C0 is responding correctly. I2C1 does not seems to work.
igorpadykov I2C1 on LVDS interface are the ones listed in the device tree and cabled on the im8qm mek. Are those i2c interface supported and functional ?
Thanks,
Stan
Hi ,
our designed board use i2c0 as lvds i2c bus,how can I modify devicetree to adjust our board ?thank you.
Hi minskey
seems there is some misunderstanding, as i.MX8QM has two lvds modules
with addresses 5724_XXX : I2C0,I2C1 and 5624_XXXX : I2C0,I2C1
described in Table 2-14. Display Interface 1 memory map, Table 2-13. Display Interface 0 memory map
i.MX8QM Reference Manual.
> 3. Can the two channels of each ldb bridge display different picture frames independently ?
not possible to support two different display sizes or timings from the same LDB.
In general may be suggested to obtain i.MX8QM Reference Manual from local marketing office.
Note i.MX8QM is not publicly released yet and has limited support.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------