IMX8QM USB OTG无法识别

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM USB OTG无法识别

274 Views
st_hw
Contributor I

你好,

最近,我遇到一个笔记本电脑无法识别IMX8QMUSB OTG设备问题。

我用IMX8QM设计制作了一个小板子A,将USB_OTG1信号引出至A板的板间连接器,将A板安装在载板B上,USB母头接口放置在B板上。将IMX8QM的boot模式调整成USB串行下载模式,使用公对公的USB线缆将B板与笔记本电脑相连。A板和B板正常上电后,在笔记本电脑的设备管理器中没有显示IMX8QM对应的USB设备。

我排查了USB线缆和电脑的USB接口,没有发现问题。排查了原理图,跟开发板相比,我只使用USB_OTG1,没有使用USB_OTG2,且我将USB_OTG1_ID上拉,目的是将IMX8QM配置成USB device。

我的问题是:如果不需要使用USB_OTG2,是否也需要将USB_OTG2_VBUS和USB_OTG2_ID做相应供电和上下拉设置。

我的部分原理图见插图。

st_hw_6-1709357828785.png

 

st_hw_5-1709357800530.png

 

st_hw_0-1709357589541.png

st_hw_1-1709357624574.pngst_hw_2-1709357677798.png

st_hw_3-1709357740610.png

感谢你的关注,期待你的解答与帮助,谢谢!

0 Kudos
2 Replies

79 Views
st_hw
Contributor I

已解决。USB数据线上不能并联TVS管。可能是TVS管选型不合适。

0 Kudos

208 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Probably it's because there is no V_BUS, could you populate the R53 to see if it gets recognized?

Regards

0 Kudos