IMX8QM-MEK: dual display configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM-MEK: dual display configuration

942 Views
vinothkumars
Senior Contributor IV

Hi All,

we are working dual display on IMX8QM-MEK platform with Yocto Linux (L5.10.52). We able to achieve dual display working as extended display but it is not working as independent displays

Following commands I have executed plays the video in primary display

gst-launch-1.0 filesrc location=file1.mp4 ! video/quicktime ! qtdemux name=d d. ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! waylandsink &

To play video on to other (secondary/extended) display need mouse pointer/cursor moved to the second display before playing the above gstreamer. Is it possible to dedicate two touch to each of the display since we have use case to support two independent operating the two displays

We could achieve independent display with QT but we would like to do the same with native wayland/weston compositor

 

@redwanmohamed 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
2 Replies

930 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

for dual lcds one can look at   i.MX Linux User’s Guide​

p.44  "Specifying displays".

 

Best regards
igor

0 Kudos
Reply

916 Views
vinothkumars
Senior Contributor IV

Hi @igorpadykov ,

 

Thank you for the reply,

 

I tried but, I unable to achieve the independent display (primary display to one user and secondary display to the other user). I am using two MIPI-DSI display.

 

Will you please provide more details on this.

 

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply