IMX8QM-MEK: DRM ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,435件の閲覧回数
vinothkumars
Senior Contributor IV

Dear All,

 

Hardware: IMX8QM-MEK

Software: Embedded Linux (L5.10.52) Weston Wayland

 

I have some questions about the DRM and DISPLAY on IMX8QM-MEK board

 

1. How many drm is present in IMX8QM-MEK board ?

    Only one drm - I am right ?

 

2. Is one drm able to support more display in independent  mode ?

   it will not support display independent mode if more than one display present and if one drm - am I right ?

 

3. Is it possible to run more than one weston client on one drm ?

   One weston Client for one drm, not more than weston client for one drm - am I right ?

 

4. Is it possible to make touch input for each display ?

   I connected two display and touch is working but I am not getting touch event for secondary display.

 

 

Will you please provide the some details or documentation for IMX8QM-MEK display (MIPI-DSI-HDMI) frame flow for along with those questions answered.

 

 

@redwan 

@DhavalS 

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
1 解決策
1,422件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

i.MX DRM drivers folow general Linux DRM framework described in documentation below

https://www.kernel.org/doc/html/latest/gpu/drm-internals.html

so may be suggested to post those questions on kernel mail list:

http://vger.kernel.org/vger-lists.html

In general i.MX8 series support multiple LCDs, one can look for example

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mq-evk-d...

Also may be useful

https://lists.freedesktop.org/archives/dri-devel/2015-May/083707.html

 

Best regards
igor

元の投稿で解決策を見る

1 返信
1,423件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

i.MX DRM drivers folow general Linux DRM framework described in documentation below

https://www.kernel.org/doc/html/latest/gpu/drm-internals.html

so may be suggested to post those questions on kernel mail list:

http://vger.kernel.org/vger-lists.html

In general i.MX8 series support multiple LCDs, one can look for example

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mq-evk-d...

Also may be useful

https://lists.freedesktop.org/archives/dri-devel/2015-May/083707.html

 

Best regards
igor