IMX8Nano DDR Tool Stuck On Waiting for board configuration from PC-end...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8Nano DDR Tool Stuck On Waiting for board configuration from PC-end...

ソリューションへジャンプ
2,431件の閲覧回数
scvi
Contributor II

Hello,

We are using a custom design board based off the 8MNANOD4-EVK. Same DRAM and PMIC

The tool successfully downloads to board but never continue after that point.

 

 

Download is complete
Waiting for the target board boot...

===================hardware_init=====================

********Found PMIC BD718XX**********
hardware_init exit

*************************************************************************

*************************************************************************

*************************************************************************
       MX8 DDR Stress Test V3.20
       Built on Feb 23 2021 13:49:21
*************************************************************************

Waiting for board configuration from PC-end...

 

 

Why would It be stuck at this step?

0 件の賞賛
返信
1 解決策
2,425件の閲覧回数
scvi
Contributor II

Turns out the UART RX on the processor was not hooked up correctly.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,426件の閲覧回数
scvi
Contributor II

Turns out the UART RX on the processor was not hooked up correctly.

0 件の賞賛
返信