IMX8Mq custom board rel_imx_4.14.98_2.0.0_ga kernel when playing video overnight , CPU freeze

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8Mq custom board rel_imx_4.14.98_2.0.0_ga kernel when playing video overnight , CPU freeze

751件の閲覧回数
agnel_terry
Contributor III

Hi ,

In our project with IMX8MQ, custom board, with Kernel and packages released to 4.14.98 , running video overnight to do performance testing ,  one or two boards have CPU freeze overnight,  couple of boards works fine for weeks with the same FW.

I am not seeing any crash in the Kernel / GStreamer debug logs. I see CPU freeze in some boards only when I start playing video. 

If I just run some frame buffer test, I am not seeing the freeze. 

As I don't have any crash messages , I am not able to get more information , will using tools like JTAG, give more Information.

Can someone help, with some information about why some boards freeze in the overnight test.

 

Thanks and regards

Terry

 

 

 

 

ラベル(1)
0 件の賞賛
7 返答(返信)

735件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

We haven't any freeze overnight in our releases with EVK board, is probably that the problem is your PMIC.

 

Regards

0 件の賞賛

715件の閲覧回数
agnel_terry
Contributor III

Hi ,

Thank you for the response,  can this issue be dubugged using  JTAG ?

Is there any VPU lock up issues reported ?

Thanks and Regards

Terry

 

 

 

 

0 件の賞賛

706件の閲覧回数
agnel_terry
Contributor III

Hi ,

In our custom board we updated the DDR from 3GB to 4GB, we ran DDR stress test and we created new lpDDR4 timing file and updated it in the U-boot, and the required changes in U-boot and kernel for the DDR is done , is there any other updates need to be done in ATF for the DDR updates.

Other than DDR is the any Power Domain driver change we need to take care for custom board , we use 4.14.98.2.0.0_GA version

 

Thanks and Regards

Terry

 

0 件の賞賛

688件の閲覧回数
agnel_terry
Contributor III

Hi 

After couple of tests, found that the video freeze only when i run on top of Weston,  using waylandsink , if I dont load weston and run the video using autovideosink, it uses KMSsink and the video runs properly, no freeze,

The unit also freeze when i run weston test application like weston-simple-egl, it runs for a while and then freeze, from this I assume  the unit freeze when the GPU is used. I assume the GPU causes the freeze, 

IS the any way I can change the GPU mem Size or is there any patch for GPU need to be dne on top of 4.14.98-2.0.0_ga.

 

Thanks and regards

Terry

 

 

 

 

 

0 件の賞賛

252件の閲覧回数
edward_fu
Contributor III

Have you resolved the problem? 

0 件の賞賛

233件の閲覧回数
agnel_terry
Contributor III

The issue was related to power rails in the board, the HW team updated the board design , we didnt see the issue after that.

0 件の賞賛

225件の閲覧回数
edward_fu
Contributor III

Thanks

0 件の賞賛