IMX8MQEVK board + wpa_supplicant - Not associating to SSID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQEVK board + wpa_supplicant - Not associating to SSID

436 Views
JKT
Contributor II

Hi,

I used the prebuilt binaries and IMX8MQEVK board boots. In that I try to use wifi (4356).

https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-EVK-Booting-LINUX-from-SD-card/td-p/1232619

lspci - lists the 4356 module.

By referring to UM11490.pdf - feature config guide for imx8mqevk)

I try to update  the /etc/wpa_supplicant.conf file. Using a open SSID, updated ssid and key_mgmt=NONE.

But when I run the wpa_supplicant -iwlan0 -Dnl80211 -c/etc/wpa_supplicant.conf 

It fails. 

It goes lot of BSS add and remove multiple times, and stuck.

wlan0: BSS: Remove id 163 BSSID f0:5c:19:8a:8d:6b SSID 'guest' due to wpa_bss_flush_by_age.

The IMX8mQEVK is not associating.

I have tried with different SSID (with and without PSK). Same status.

why is this behavior? and how to resolve this?

 

Regards.

 

 

 

 

 

 

 

0 Kudos
1 Reply

421 Views
igorpadykov
NXP Employee
NXP Employee

Hi JKT

 

one can look at linux wifi documentation on

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

 

Best regards
igor

0 Kudos