IMX8MQ wifi not starting in Linux os

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ wifi not starting in Linux os

672 Views
Manikandan
Contributor II

Hi,

I have  started working with IMX8M EVK. I'm trying make IMX8MQ EVK as Access point

but i'm facing some issues like the below ERROR i'm getting

--------------------------------------------------------------------------------------------------------------------------------------

root@imx8mqevk:~# hostapd /etc/hostapd.conf
Configuration file: /etc/hostapd.conf
rfkill: Cannot open RFKILL control device
ACS: Automatic channel selection started, this may take a bit
wlan0: interface state UNINITIALIZED->ACS
wlan0: ACS-STARTED
ACS: Unable to collect survey data
ACS: All study options have failed
Interface initialization failed
wlan0: interface state ACS->DISABLED
wlan0: AP-DISABLED
ACS: Possibly channel configuration is invalid, please report this along with your config file.
ACS: Failed to start
wlan0: AP-DISABLED
hostapd_free_hapd_data: Interface wlan0 wasn't started
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
wlan0: interface state DISABLED->DISABLED
wlan0: interface state DISABLED->DISABLED
wlan0: AP-DISABLED
wlan0: CTRL-EVENT-TERMINATING
hostapd_free_hapd_data: Interface wlan0 wasn't started

-----------------------------------------------------------------------------------------------------------------------------------------

suggest me how to resolve this issue.

0 Kudos
1 Reply

660 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Which bsp version and wifi you are using ? WLAN driver except MARVELL in BSP Version L5.xx is disabled in kernel.

 

BR

Zhiming

0 Kudos