IMX8MQ gst vpudec Could not initialize supporting library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ gst vpudec Could not initialize supporting library

Jump to solution
12,475 Views
cedric_thamin
Contributor III

Hi

I have an issue with vpudec ... It never work for me ...

I have no idea what is good way for fixing it ...

 

Traces :
GST_DEBUG=3 gst-launch-1.0 filesrc location=/tmp/a/video/less_small.mp4 ! 'video/quicktime' ! aiurdemux ! 'video/x-h264,weigth=480,height=270' ! vpudec ! glimagesink
Setting pipeline to PAUSED ...
====== VPUDEC: 4.5.1 build on Jul 9 2020 15:00:11. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jul 9 2020 11:12:16)
vpulib: 1.1.1
firmware: 1.1.1.65535
0:00:00.196885888 4941 0xaaaad469f230 ERROR default gstallocatorphymem.c:149:base_alloc: Allocate phymem 16777232 failed.

0:00:00.196947088 4941 0xaaaad469f230 ERROR default gstvpu.c:90:gst_vpu_allocate_internal_mem: Could not allocate memory using VPU allocator
0:00:00.197042608 4941 0xaaaad469f230 ERROR vpu_dec_object gstvpudecobject.c:338:gst_vpu_dec_object_start:<vpudecobject0> gst_vpu_allocate_internal_mem fail
0:00:00.197073088 4941 0xaaaad469f230 WARN videodecoder gstvideodecoder.c:2533:gst_video_decoder_change_state:<vpudec0> error: Failed to start decoder
ERROR: Pipeline doesn't want to pause.
Got context from element 'sink': gst.gl.GLDisplay=context, gst.gl.GLDisplay=(GstGLDisplay)"\(GstGLDisplayVivFB\)\ gldisplayvivfb0";
ERROR: from element /GstPipeline:pipeline0/GstVpuDec:vpudec0: Could not initialize supporting library.
Additional debug info:
../../../../git/gst-libs/gst/video/gstvideodecoder.c(2533): gst_video_decoder_change_state (): /GstPipeline:pipeline0/GstVpuDec:vpudec0:
Failed to start decoder
Setting pipeline to NULL ...
Freeing pipeline ...

 

Some information which can help you for helping me :

# uname -a
Linux  4.19.35-sdtv-warrior-conf #1 SMP PREEMPT Mon Sep 21 10:32:38 UTC 2020 aarch64 GNU/Linux

# cat /proc/meminfo | grep Cma
CmaTotal: 983040 kB
CmaFree: 709652 kB

# gst-inspect-1.0 --version
gst-inspect-1.0 version 1.16.0
GStreamer 1.16.0
Unknown package origin

# gst-launch-1.0 --version
gst-launch-1.0 version 1.16.0
GStreamer 1.16.0
Unknown package origin

What can I add ?

Thanks for your help
Best regards,
Cedric T

 

0 Kudos
Reply
1 Solution
12,412 Views
cedric_thamin
Contributor III

Hi igorpadykov

 

Yes with official bsp it is working. My issue come from my integration in my yocto env.

I found the issue and for other user I will try explain my issue.

1 - What was my problem :

VPUdec gstreamer module failed to malloc memory

2 - My fix :

I must to synchronised all these recipes to same bsp version (me i synchronized with warrior version)

linux-imx
inux-imx-headers
imx-vpuwrap
imx-vpu-hantro

And in conf/machine/include/imx-base.inc check var MACHINEOVERRIDES_EXTENDER_mx8mq, imxvpuhantro should be inside it.

 

3 - Why I met these issues

My yocto env was created for raspberry board, and more later I had support for nxp board.
My reference was poky version thud. But I met an issue with nxp tee with this version so I upgrade kernel, optee-os, optee-client to warrior version for fixed it.
linux-imx and inux-imx-headers was not more synchronised and vpu didnt work anymore

4 - Some line for testing vpu:
This two line is working for me now.

Add package imx-test
/unit_tests/VPU/hantro/hx170dec -Oout /tmp/a/video/15.Papaoutai.avi

With gstreamer
GST_DEBUG=3 gst-launch-1.0 filesrc location=/tmp/a/video/less_small.mp4 ! 'video/quicktime' ! aiurdemux ! 'video/x-h264,weigth=480,height=270' ! vpudec ! glimagesink


Best regards,
Cedric T

View solution in original post

0 Kudos
Reply
9 Replies
11,976 Views
valeraghost
Contributor I

Hi,cedric_thamin, I have the same problem with imx8mp custom board and yocto zeus linux.

Could you provide detailed instruction what to do to make it work, How to syncronise versions? do  i have  to rebuild the image.

i  try to follow this instruction to build (because i have solidrun kit).

https://github.com/SolidRun/meta-solidrun-arm-imx8/tree/zeus-imx8mp

0 Kudos
Reply
11,949 Views
cedric_thamin
Contributor III

Hi

For this package list you should compare version build in you env and in official BSP:
linux-imx
inux-imx-headers
imx-vpuwrap
imx-vpu-hantro


As example for identify build version of imx-vpuwrap i do :  ls tmp/work/aarch64-mx8m-poky-linux/imx-vpuwrap

You can compare so output of command bitbake -e package_name in you env and in official bsp for each package.
I don't know your chip, perhaps it is not same vpu ...check if you need of this flag : imxvpuhantro
and check if it is activated:

bitbake -e imx-vpuwrap | grep imxvpuhantro
You should have this list of var with flag imxvpuhantro
MACHINEOVERRIDES="imx:mx8:mx8m:imxdrm:imxvpu:imxvpuhantro:imxgpu:imxgpu3d:mx8mq:imx8mqevk:aarch64"
MACHINEOVERRIDES_EXTENDER="imxdrm:imxvpu:imxvpuhantro:imxgpu:imxgpu3d"
MACHINEOVERRIDES_EXTENDER_mx8mq="imxdrm:imxvpu:imxvpuhantro:imxgpu:imxgpu3d"
OVERRIDES="linux:aarch64:pn-imx-vpuwrap:imx:mx8:mx8m:imxdrm:imxvpu:imxvpuhantro:imxgpu:imxgpu3d:mx8mq:imx8mqevk:aarch64:poky:class-target:libc-glibc:forcevariable"

Good luck
Cedric Thamin

0 Kudos
Reply
12,456 Views
cedric_thamin
Contributor III

Hi

Thanks for your attention.

Try with Demo Images from

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

I can not. My board is a cutom board and official test image is not working on it.

https://variwiki.com/index.php?title=DART-MX8M_GSTREAMER&release=RELEASE_SUMO_V2.1_DART-MX8M

I tried two examples chap 5
gst-launch-1.0 playbin uri=file:/tmp/a/video/Big_Buck_Bunny_1080_10s_2MB.mp4
Video was played. In we can see it failed to used vpudec and use avdec_h264
Please see trace playbin.txt

gst-launch-1.0 filesrc location=/run/media/sda1/big_buck_bunny.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! autovideosink
No video was played.
See trace vpudec.txt

I don't understand why gstallocatorphymem.c:149:base_alloc: Allocate phymem 16777232 failed. it is normal? I can not compare with a working board

0 Kudos
Reply
12,446 Views
igorpadykov
NXP Employee
NXP Employee

Please try Demo Images from below link with NXP i.MX8MQ EVK board

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

What bsp used in your case, which reference design is based your board.

If it is based on i.MX8MQ EVK board one can rebuild image for custom board using

linux documentation on above link.

 

Best regards
igor

0 Kudos
Reply
12,413 Views
cedric_thamin
Contributor III

Hi igorpadykov

 

Yes with official bsp it is working. My issue come from my integration in my yocto env.

I found the issue and for other user I will try explain my issue.

1 - What was my problem :

VPUdec gstreamer module failed to malloc memory

2 - My fix :

I must to synchronised all these recipes to same bsp version (me i synchronized with warrior version)

linux-imx
inux-imx-headers
imx-vpuwrap
imx-vpu-hantro

And in conf/machine/include/imx-base.inc check var MACHINEOVERRIDES_EXTENDER_mx8mq, imxvpuhantro should be inside it.

 

3 - Why I met these issues

My yocto env was created for raspberry board, and more later I had support for nxp board.
My reference was poky version thud. But I met an issue with nxp tee with this version so I upgrade kernel, optee-os, optee-client to warrior version for fixed it.
linux-imx and inux-imx-headers was not more synchronised and vpu didnt work anymore

4 - Some line for testing vpu:
This two line is working for me now.

Add package imx-test
/unit_tests/VPU/hantro/hx170dec -Oout /tmp/a/video/15.Papaoutai.avi

With gstreamer
GST_DEBUG=3 gst-launch-1.0 filesrc location=/tmp/a/video/less_small.mp4 ! 'video/quicktime' ! aiurdemux ! 'video/x-h264,weigth=480,height=270' ! vpudec ! glimagesink


Best regards,
Cedric T

0 Kudos
Reply
11,744 Views
mb1
Contributor III

I ran into the same error. All necessary packages were in place, but I still got the same error.

 

GST_DEBUG=3 gst-launch-1.0 v4l2src device=/dev/video2 ! "video/x-raw, format=NV12, wid
th=1920, height=1080, framerate=30/1" ! vpuenc_h264 ! mpegtsmux name=mux ! filesink location=test_1080.t
s
[ 2105.945005] enter isp_mi_stop
Setting pipeline to PAUSED ...
0:00:00.262886750  2019 0xaaab28ff2d20 WARN                    v4l2 v4l2_calls.c:547:gst_v4l2_subscribe_
event:<v4l2src0> Cannot subscribe V4L2_EVENT_SOURCE_CHANGE or V4L2_EVENT_EOS event for device '/dev/vide
o2'.
====== VPUENC: 4.6.1 build on Aug 12 2021 12:58:31. ======
        wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Aug 12 2021 12:10:18)
        vpulib: 1.1.1
        firmware: 1.1.1.43691
0:00:00.263479000  2019 0xaaab28fea2a0 WARN                 v4l2src gstv4l2src.c:694:gst_v4l2src_query:<
v4l2src0> Can't give latency since framerate isn't fixated !
0:00:00.263520750  2019 0xaaab28fea2a0 WARN              aggregator gstaggregator.c:1990:gst_aggregator_
query_latency_unlocked:<mux> Latency query failed
0:00:00.263933000  2019 0xaaab28ff2d20 ERROR                default gstallocatorphymem.c:150:base_alloc:
 Allocate phymem 10485776 failed.

0:00:00.263961000  2019 0xaaab28ff2d20 ERROR                default gstvpu.c:90:gst_vpu_allocate_interna
l_mem: Could not allocate memory using VPU allocator
0:00:00.263985000  2019 0xaaab28ff2d20 ERROR                 vpuenc gstvpuenc.c:556:gst_vpu_enc_start:<v
puenc_h264-0> gst_vpu_allocate_internal_mem fail
0:00:00.264012000  2019 0xaaab28ff2d20 WARN            videoencoder gstvideoencoder.c:1781:gst_video_enc
oder_change_state:<vpuenc_h264-0> error: Failed to start encoder
ERROR: from element /GstPipeline:pipeline0/vpuenc_h264:vpuenc_h264-0: Could not initialize supporting li
brary.
Additional debug info:
../git/gst-libs/gst/video/gstvideoencoder.c(1781): gst_video_encoder_change_state (): /GstPipeline:pipel
ine0/vpuenc_h264:vpuenc_h264-0:
Failed to start encoder
ERROR: pipeline doesn't want to preroll.
Failed to set pipeline to PAUSED.
Setting pipeline to NULL ...
Freeing pipeline ...

 


I figured out the VPUDEC failure came with the stripped defconfig I used. The VPU in KConfig seems to miss a dependency.

The three neccessary config values are:

CONFIG_ION=y
CONFIG_ION_SYSTEM_HEAP=y
CONFIG_ION_CMA_HEAP=y

 

Best Regards

0 Kudos
Reply
10,224 Views
caiortp
Contributor I

Hi ,

After enabling the

CONFIG_ION=y
CONFIG_ION_SYSTEM_HEAP=y
CONFIG_ION_CMA_HEAP=y

The error is gone

default gstvpu.c:90:gst_vpu_allocate_interna l_mem: Could not allocate memory using VPU allocator

But the CPU consumption is very high, around 75% on imx8mm running the demo

GST_DEBUG=3 gst-launch-1.0 videotestsrc ! video/x-raw, format=I420, width=640, height=480 ! vpuenc_h264 ! filesink location=test.mp4 

 

Best Regards,

0 Kudos
Reply
9,139 Views
mb1
Contributor III

I ran into this issue - again.

I then figured out, that CONFIG_ION support was removed in Linux 5.11.

The config options making it work for Kernel > 5.11 are now:

 

 

CONFIG_DMABUF_HEAPS=y
CONFIG_DMABUF_HEAPS_SYSTEM=y
CONFIG_DMABUF_HEAPS_CMA=y