IMX8MQ: compatible LPDDR4 devices?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ: compatible LPDDR4 devices?

518 Views
N_Coesel
Contributor III

Hello,

I'm running into trouble finding Micron memory for an IMX8MQ design. I have used the same part ( MT53E768M32D4DT-053 WT:E ) which is on the IMX8MQ EVK board but this isn't available anywhere. The same goes for any LPDDR device from Micron with a similar capacity (2GB to 4GB; I don't care right now). Are there any alternatives out there which are available?

thanks in advance!

0 Kudos
1 Reply

423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nico

file was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos