IMX8MQ Uboot2021.04 supports uboot OLED logo display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ Uboot2021.04 supports uboot OLED logo display

221 Views
pyh0603
Contributor III

Hello,
Release: android_p11.0.0_2.6.0
Board: i.MX8MQ based custom board
OLED:RM67191

 

My reference link:

https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-DSI-host-controller-support-at-U-boot/m-p/102319...

I have already implemented LCD logo display in Uboot in image android_p9.0.0_1.0.0-ga_image_8mqevk.tar.gz, but it uses Uboot version 2018.03, while I am currently using Uboot version 2021.04 in image android_p11.0.0_2.6.0. There is a significant difference between the two uboot versions. 

Is there a patch for version uboot.2021.04 available?

Looking forward to your reply

 

0 Kudos
Reply
1 Reply

198 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can check all relevant uboot in NXP github:

https://github.com/nxp-imx/uboot-imx

Regards

0 Kudos
Reply