IMX8MQ HDMI detection at U-Boot level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MQ HDMI detection at U-Boot level

2,124件の閲覧回数
hiteshviradiya
Contributor III

Dear NXP team,

We have designed our custom product based on imx8mq SoC and we are good with the things nowadays.

We want to detect HDMI at u-boot level. How can it be done ?

On our imx6 base product we are already using it and we have usecase for this and in imx6 u-boot

struct display_info_t structure in board file have

.detect = hdmi_detect

but in imx8mq u-boot it is NULL. And hence u-boot is always default to HDMI irrespective of HDMI monitor is connected or not.

Please advise how to achieve our usecase of detecting HDMI at uboot level.

--

Thanks,

Hitesh

0 件の賞賛
返信
1 返信

1,985件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hitesh

some hdmi related codes are provided in uboot:

imx8mq_evk.c\imx8mq_evk\freescale\board - uboot-imx - i.MX U-Boot 

edid detection codes can be reused from linux sources, one can look

at sect.6.4.6 High-Definition Multimedia Interface (HDMI) and Display
Port (DP) Overview attached Linux Manual.

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信