IMX8MQ-EVK with Flashing eMMC issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ-EVK with Flashing eMMC issue

Jump to solution
320 Views
Ichi_
Contributor I

Environment and Device:

    1.imx8mq evk

    2.Linux 6.6.23_2.0.0 bitbake imx-image-core

    3.build file

       3.1 imx-boot-imx8mqevk-sd.bin-flash_evk

       3.2 imx-image-core-imx8mqevk.rootfs-20240906101159.wic

issue: I tried two way to burn the eMMC but all failed.

    1. use uuu.auto(uuu_version 1.2.39)

       continuous run 2:2-NXP from 0 to 100% and won't stop.

      IChi__0-1725944367655.png

    2. uuu -v -b emmc_all imx-boot-imx8mqevk-sd.bin-flash_evk imx-image-core-  imx8mqevk.rootfs-20240906101159.wic

     IChi__1-1725944703036.png

     continuous run 2:2-NXP 100% too.

Thank for any help.

        

 

 

0 Kudos
Reply
1 Solution
277 Views
Harvey021
NXP TechSupport
NXP TechSupport

Have a try use the one:
uuu -v -b emmc_all imx-boot-imx8mq-evk-sd.bin-flash_evk imx-image-core-imx8mqevk.rootfs-20240906101159.wic

or uuu -v -b emmc_all  imx-image-core-imx8mqevk.rootfs-20240906101159.wic

 

Regards

Harvey

View solution in original post

0 Kudos
Reply
3 Replies
278 Views
Harvey021
NXP TechSupport
NXP TechSupport

Have a try use the one:
uuu -v -b emmc_all imx-boot-imx8mq-evk-sd.bin-flash_evk imx-image-core-imx8mqevk.rootfs-20240906101159.wic

or uuu -v -b emmc_all  imx-image-core-imx8mqevk.rootfs-20240906101159.wic

 

Regards

Harvey

0 Kudos
Reply
267 Views
Ichi_
Contributor I

Hi Harvey021

Burning has been successfull when using ILF_v6.6.23-2.0.0_images_IMX8MQEVK-> 

imx-boot-imx8mq-evk-sd.bin-flash_evk + imx-image-core-imx8mqevk.rootfs-

20240906101159.wicfile.

 

But my build folder no imx-boot-imx8mq-evk-sd.bin-flash_evk file,

only imx-boot-imx8mq-evk-sd.bin-flash_evk. Is this correct?

IChi__0-1725961920548.png

 

 

 

0 Kudos
Reply
247 Views
Harvey021
NXP TechSupport
NXP TechSupport

Build it by changing the MACHINE to imx8mq-evk as provided - meta-freescale/conf/machine/

Or to download it from prebuild image (IMXLINUX) will be time saving.

 

Regards

Harvey

 

0 Kudos
Reply