IMX8MQ EVK ENET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MQ EVK ENET

1,415 Views
haochengdong
Contributor II

Why does NVK_ENET_2V5 of EVK provide current from VDDIO_REG of AR8031? Can the power supply capacity of AR8031 meet the requirements? Are there any other power-on timing requirements? Our product wants to use the VGEN6 of MC34PF4210 to power NVCC_ENET_2V5. Is this feasible?

0 Kudos
Reply
1 Reply

1,339 Views
mrudangshelat1
Senior Contributor II

Hi,

NVCC_ENET_2V5 can be provided from VDDIO_REG of AR8031 as NVCC_ENET_2V5 is just an IO voltage for IO pin. And it consumes very little current.

As per iMX8M power sequence, all NVCC (including Enet) rails must be powered up at seq 6. The VGEN6 LDO in PMIC is at power seq 7. The PMIC VGEN6 voltage in all OTP configurations is 2.8V which needs to reduce to 2.5V for AR8031. Instead, AR8031 supports the internal regulator to support 2.5V.

Regards,

Mrudang

 

0 Kudos
Reply