I am trying to figure out a wifi issue on Android which causes the system to be crashed and rebooted. When I have a wifi connection or even search for available networks, suddenly the system is restarted due to some reason. Is there anyone who can shed some light on how I can debug or solve the issue?
here are the logcat output AND the system log before restart:
the system log is pretty interesting and according to that log seems there is an issue related to memory
=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2023.01.29 01:23:54 =~=~=~=~=~=~=~=~=~=~=~=
em_sbc_imx8m:/ $ [ 598.627331] init: Received control message 'start' for 'wpa_supplicant' from pid: 2996 (/system/bin/wificond)
[ 598.654545] init: starting service 'wpa_supplicant'...
[ 598.661453] type=1400 audit(1578552645.574:3652): avc: denied { read } for pid=2962 comm="health@2.0-serv" name="stat" dev="sysfs" ino=21542 scontext=u:r:hal_health_default:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=0 duplicate messages suppressed
[ 598.675601] init: Created socket '/dev/socket/wpa_wlan0', mode 660, user 1010, group 1010
[ 598.694622] type=1400 audit(1578552685.274:3653): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 599.217567] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 602.779618] init: processing action (sys.sysctl.tcp_def_init_rwnd=*) from (/init.rc:729)
[ 608.642709] type=1400 audit(1578552685.274:3656): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0 duplicate messages suppressed
[ 608.662384] type=1400 audit(1674955465.089:3657): avc: denied { read } for pid=2962 comm="health@2.0-serv" name="stat" dev="sysfs" ino=21542 scontext=u:r:hal_health_default:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=0
[ 613.491883] Unable to handle kernel NULL pointer dereference at virtual address 00000000
[ 613.500120] Mem abort info:
[ 613.502923] Exception class = DABT (current EL), IL = 32 bits
[ 613.509025] SET = 0, FnV = 0
[ 613.512103] EA = 0, S1PTW = 0
[ 613.515267] Data abort info:
[ 613.518228] ISV = 0, ISS = 0x00000004
[ 613.522073] CM = 0, WnR = 0
[ 613.525288] user pgtable: 4k pages, 48-bit VAs, pgd = ffff800064dc7000
[ 613.532038] [0000000000000000] *pgd=0000000000000000
[ 613.537088] Internal error: Oops: 96000004 [#1] PREEMPT SMP
[ 613.542661] Modules linked in: brcmfmac brcmutil
[ 613.547284] CPU: 3 PID: 4129 Comm: wpa_supplicant Not tainted 4.14.78-00007-gf2ee4949105b #1
[ 613.555719] Hardware name: Freescale i.MX8MQ EVK (DT)
[ 613.560770] task: ffff800006ea9c00 task.stack: ffff00000a570000
[ 613.566791] PC is at brcmf_p2p_send_action_frame+0x1ec/0x818 [brcmfmac]
[ 613.573489] LR is at brcmf_p2p_send_action_frame+0x1dc/0x818 [brcmfmac]
[ 613.580104] pc : [<ffff000001019474>] lr : [<ffff000001019464>] pstate: 80000145
[ 613.587498] sp : ffff00000a573780
[ 613.590813] x29: ffff00000a573780 x28: 0000000000000001
[ 613.596127] x27: 0000000000000000 x26: 0000000000000000
[ 613.601441] x25: ffff8000793ec900 x24: 00000000ffffffff
[ 613.606756] x23: ffff800007d1401c x22: ffff800007d14000
[ 613.612071] x21: ffff8000793eb7a0 x20: ffff8000793eb7c0
[ 613.617385] x19: ffff8000793eb7b8 x18: 000000000000007e
[ 613.622700] x17: 0000e104d14f32e0 x16: ffff000008d2847c
[ 613.628015] x15: 0000000000000003 x14: 9180b21a7ec0ac88
[ 613.633329] x13: 000000d000330033 x12: 006c0004000003e8
[ 613.638644] x11: 00570008000015b8 x10: 0000000000000040
[ 613.643959] x9 : 0000000000000000 x8 : 0801070106010200
[ 613.649273] x7 : 0a0100000e000002 x6 : ffff800007d14033
[ 613.654587] x5 : 0000000000000040 x4 : 0000000000000004
[ 613.659901] x3 : 0000000000000080 x2 : 0000000000001400
[ 613.665216] x1 : ffff8000793eb7c0 x0 : 0000000000000000
[ 613.670531]
[ 613.670531] X1: 0xffff8000793eb740:
[ 613.675496] b740 793ed018 ffff8000 09e23000 ffff0000 092641a0 ffff0000 00000000 00000000
[ 613.683688] b760 0102e808 ffff0000 00000000 00000000 00000001 00000000 00010000 0000000e
[ 613.691879] b780 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.700070] b7a0 793eb300 ffff8000 79e1a800 ffff8000 79997e80 ffff8000 793eb7a0 ffff8000
[ 613.708262] b7c0 00001400 00000000 00000000 00000000 00000000 00000000 793ed000 ffff8000
[ 613.716452] b7e0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.724642] b800 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.732833] b820 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.741026]
[ 613.741026] X6: 0xffff800007d13fb3:
[ 613.745990] 3fb0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.754181] 3fd0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.762372] 3ff0 00000000 00000000 00000000 00000000 00000070 00000190 7ec0ac88 0000b21a
[ 613.770563] 4010 7ec0ac88 0017b21a 00000000 6c000a04 0e000002 0a010000 06010200 08010701
[ 613.778754] 4030 00010c01 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.786944] 4050 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.795134] 4070 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.803325] 4090 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.811516] 40b0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.819713]
[ 613.819713] X19: 0xffff8000793eb738:
[ 613.824763] b738 793ed018 ffff8000 793ed018 ffff8000 09e23000 ffff0000 092641a0 ffff0000
[ 613.832949] b758 00000000 00000000 0102e808 ffff0000 00000000 00000000 00000001 00000000
[ 613.841133] b778 00010000 0000000e 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.849316] b798 00000000 00000000 793eb300 ffff8000 79e1a800 ffff8000 79997e80 ffff8000
[ 613.857500] b7b8 793eb7a0 ffff8000 00001400 00000000 00000000 00000000 00000000 00000000
[ 613.865683] b7d8 793ed000 ffff8000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.873867] b7f8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.882050] b818 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.890234]
[ 613.890234] X20: 0xffff8000793eb740:
[ 613.895284] b740 793ed018 ffff8000 09e23000 ffff0000 092641a0 ffff0000 00000000 00000000
[ 613.903468] b760 0102e808 ffff0000 00000000 00000000 00000001 00000000 00010000 0000000e
[ 613.911651] b780 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.919835] b7a0 793eb300 ffff8000 79e1a800 ffff8000 79997e80 ffff8000 793eb7a0 ffff8000
[ 613.928019] b7c0 00001400 00000000 00000000 00000000 00000000 00000000 793ed000 ffff8000
[ 613.936202] b7e0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.944386] b800 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.952569] b820 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.960754]
[ 613.960754] X21: 0xffff8000793eb720:
[ 613.965803] b720 7ab03a80 ffff8000 00000000 00000000 00000000 00000000 793ed018 ffff8000
[ 613.973986] b740 793ed018 ffff8000 09e23000 ffff0000 092641a0 ffff0000 00000000 00000000
[ 613.982170] b760 0102e808 ffff0000 00000000 00000000 00000001 00000000 00010000 0000000e
[ 613.990353] b780 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 613.998537] b7a0 793eb300 ffff8000 79e1a800 ffff8000 79997e80 ffff8000 793eb7a0 ffff8000
[ 614.006720] b7c0 00001400 00000000 00000000 00000000 00000000 00000000 793ed000 ffff8000
[ 614.014904] b7e0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.023087] b800 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.031272]
[ 614.031272] X22: 0xffff800007d13f80:
[ 614.036321] 3f80 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.044504] 3fa0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.052688] 3fc0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.060872] 3fe0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.069055] 4000 00000070 00000190 7ec0ac88 0000b21a 7ec0ac88 0017b21a 00000000 6c000a04
[ 614.077239] 4020 0e000002 0a010000 06010200 08010701 00010c01 00000000 00000000 00000000
[ 614.085423] 4040 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.093606] 4060 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.101790]
[ 614.101790] X23: 0xffff800007d13f9c:
[ 614.106839] 3f9c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.115023] 3fbc 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.123206] 3fdc 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.131390] 3ffc 00000000 00000070 00000190 7ec0ac88 0000b21a 7ec0ac88 0017b21a 00000000
[ 614.139573] 401c 6c000a04 0e000002 0a010000 06010200 08010701 00010c01 00000000 00000000
[ 614.147757] 403c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.155941] 405c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.164124] 407c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.172309]
[ 614.172309] X25: 0xffff8000793ec880:
[ 614.177358] c880 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.185542] c8a0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.193725] c8c0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.201908] c8e0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 614.210092] c900 76190000 ffff8000 793ed000 ffff8000 793ec000 ffff8000 00000080 00000000
[ 614.218276] c920 793ec920 ffff8000 793ec920 ffff8000 0101b520 ffff0000 00000080 00000000
[ 614.226460] c940 793ec940 ffff8000 793ec940 ffff8000 0101b390 ffff0000 00000000 00000000
[ 614.234644] c960 00000000 00000000 fb339180 0000030d 00010001 00000000 00040004 00000000
[ 614.242829]
[ 614.244320] Process wpa_supplicant (pid: 4129, stack limit = 0xffff00000a570000)
[ 614.251713] Call trace:
[ 614.254159] Exception stack(0xffff00000a573640 to 0xffff00000a573780)
[ 614.260599] 3640: 0000000000000000 ffff8000793eb7c0 0000000000001400 0000000000000080
[ 614.268427] 3660: 0000000000000004 0000000000000040 ffff800007d14033 0a0100000e000002
[ 614.276255] 3680: 0801070106010200 0000000000000000 0000000000000040 00570008000015b8
[ 614.284083] 36a0: 006c0004000003e8 000000d000330033 9180b21a7ec0ac88 0000000000000003
[ 614.291912] 36c0: ffff000008d2847c 0000e104d14f32e0 000000000000007e ffff8000793eb7b8
[ 614.299740] 36e0: ffff8000793eb7c0 ffff8000793eb7a0 ffff800007d14000 ffff800007d1401c
[ 614.307568] 3700: 00000000ffffffff ffff8000793ec900 0000000000000000 0000000000000000
[ 614.315396] 3720: 0000000000000001 ffff00000a573780 ffff000001019464 ffff00000a573780
[ 614.323225] 3740: ffff000001019474 0000000080000145 0000000000000000 0000000180100010
[ 614.331053] 3760: 0000ffffffffffff 0000000000000017 ffff00000a573780 ffff000001019474
[ 614.338957] [<ffff000001019474>] brcmf_p2p_send_action_frame+0x1ec/0x818 [brcmfmac]
[ 614.346667] [<ffff00000101070c>] brcmf_cfg80211_mgmt_tx+0x1cc/0x270 [brcmfmac]
[ 614.353892] [<ffff000008f37a34>] cfg80211_mlme_mgmt_tx+0x100/0x3a8
[ 614.360074] [<ffff000008f2c6a4>] nl80211_tx_mgmt+0x25c/0x358
[ 614.365734] [<ffff000008d970e8>] genl_family_rcv_msg+0x244/0x36c
[ 614.371739] [<ffff000008d972a8>] genl_rcv_msg+0x98/0xcc
[ 614.376963] [<ffff000008d96770>] netlink_rcv_skb+0xdc/0x118
[ 614.382534] [<ffff000008d96e90>] genl_rcv+0x34/0x48
[ 614.387411] [<ffff000008d95de4>] netlink_unicast+0x1e0/0x288
[ 614.393068] [<ffff000008d96240>] netlink_sendmsg+0x2d8/0x398
[ 614.398729] [<ffff000008d25248>] sock_sendmsg+0x44/0x50
[ 614.403954] [<ffff000008d25944>] ___sys_sendmsg+0x280/0x2b4
[ 614.409525] [<ffff000008d2852c>] SyS_sendmsg+0xb0/0xe0
[ 614.414661] Exception stack(0xffff00000a573ec0 to 0xffff00000a574000)
[ 614.421101] 3ec0: 0000000000000007 0000ffffdbd232b0 0000000000000000 0000000000000001
[ 614.428929] 3ee0: 0000e104d10552a0 0000e104d10558c0 0000000000000000 0000000000000000
[ 614.436757] 3f00: 00000000000000d3 0000000000000000 000000000000000c 0000000b00000003
[ 614.444585] 3f20: 0000000000000000 0000000000000000 000000000000000d 0000000000000003
[ 614.452413] 3f40: 0000e104d15fea20 0000e104d14f32e0 000000000000007e 0000e104d1031840
[ 614.460241] 3f60: 0000e104d103c550 0000e104d23dd5e0 0000e104d10551c0 0000e104d10557e0
[ 614.468070] 3f80: 0000e104d10286f0 000000000000002f 0000e104d23dd5e0 0000000000000001
[ 614.475898] 3fa0: 0000e104d23dd5e0 0000ffffdbd23330 0000e104d15cb210 0000ffffdbd232b0
[ 614.483726] 3fc0: 0000e104d14f32e8 0000000040000000 0000000000000007 00000000000000d3
[ 614.491554] 3fe0: 0000000000000000 0000000000000000 0000000000000000 0000000000000000
[ 614.499384] [<ffff000008083ac0>] el0_svc_naked+0x34/0x38
[ 614.504696] Code: 394016e0 7100081f 54000aa0 f9401a60 (f9400000)
[ 614.510793] ---[ end trace 4c6faa16ef08ec56 ]---
[ 614.515410] Kernel panic - not syncing: Fatal exception
[ 614.520634] SMP: stopping secondary CPUs
[ 614.525085] Kernel Offset: disabled
[ 614.528572] CPU features: 0x080200c
[ 614.532058] Memory Limit: none
[ 614.535113] Rebooting in 5 seconds..
U-Boot SPL 2018.03-gb008f48c58 (Jan 09 2020 - 03:50:02 +0000)
power_bd71837_init
set buck8 to 1.2v for DDR4
DDRINFO: start lpddr4 ddr init
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 1600MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 1064MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
U-Boot 2018.03-gb008f48c58 (Jan 09 2020 - 03:50:02 +0000)
CPU: Freescale i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 45C
Reset cause: POR
Model: Freescale i.MX8MQ EVK
DRAM: 2 GiB
tcpc_init: Can't find device id=0x50
setup_typec: tcpc init failed, err=-19
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment
Failed (-5)
No panel detected: default to HDMI
Display: HDMI (1280x720)
In: serial
Out: serial
Err: serial
BuildInfo:
- ATF d6451cc
- U-Boot 2018.03-gb008f48c58
flash target is MMC:0
N