IMX8MQ 8G LPDDR4 change

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MQ 8G LPDDR4 change

跳至解决方案
891 次查看
coindu
Contributor IV

Hi community:

        I have a qustion about use 8G LPDDR4 instead of 3G lpddr4 on IM8MQ.

       Firstly download the laster ddr tools with mscale_ddr_tool _v3.20 and MX8M_LPDDR4_RPA_v29.xlsx.

       Then open the DDR datasheet, I can see the below infomation

coindu_0-1626232571266.png

 

       row aaddress is [16:0]

       so I modify the RPA file 

       

coindu_1-1626232622555.png

        copy DDR strees test file to xxxx.ds and run the mscale DDR tool. the result is raw 16, something wrong?   Does the tool can support to 8G?

        

coindu_2-1626232728002.png

    and how the modify the uboot code about it. 

标签 (1)
0 项奖励
1 解答
884 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Coin

 

unfortunately lpddr4 devices with 17-row addresses are not supported by i.MX8MQ.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
2 回复数
885 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Coin

 

unfortunately lpddr4 devices with 17-row addresses are not supported by i.MX8MQ.

 

Best regards
igor

0 项奖励
879 次查看
coindu
Contributor IV

        Does it means that 8G DDR cannot be support?According to the chip manual, it supports 8GLPDDR configuration.Do you have any successful experience with 8G LPDDR?

标记 (1)
0 项奖励