IMX8MPLUS - MIPI CSI-2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MPLUS - MIPI CSI-2

9,154件の閲覧回数
YoavBenita
Contributor II

Hi,

I am designing board with IMX8M PLUS and want to connect 2 camera sensors (AAA0556NXX).

This sensor is using MIPI CSI-2 for the data.

As I understand, the it can be connected directly, without external terminations. Am I right ?

Both camera data will be compress by the IMX, and transmit the data to other processor (Polarfire - FPGA).

I want to use the DSI channel for the data transfer, is it possible ? should I consider any important roles ?

Thanks !

0 件の賞賛
返信
6 返答(返信)

9,135件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Yoav Benita,

For a detailed information about MIPI-CSI connection please check i.MX 8M Plus EVK Base Board Design Files, on page 12 of SPF-46370_B1.pdf ''Camera CSI Interface'' there are all the recommended schematics for MIPI-CSI connections.

Also, it could be possible to transmit your images from the cameras to your FPGA using MIPI-DSI the only that you need to consider is that your FPGA is able to receive that information and process it. 

Best regards.

0 件の賞賛
返信

9,123件の閲覧回数
YoavBenita
Contributor II
Hi,

As I saw in the EVK, there is no external resistors for termination, but this design files do not include the internal SoM schematic (IMX, PMIC, DDR etc). So it hard to understand, according to the EVK, if external termination is required.

Same about the DSI.

Can you refer me to the relevant document ?

Thank you !
0 件の賞賛
返信

9,117件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Yoav Benita,

Sure, here is attached the schematic for the SOM board.

MIPI-CSI and MIPI-DSI connections are on page 7.

Best regards.

0 件の賞賛
返信

9,110件の閲覧回数
YoavBenita
Contributor II

Thank you Jurge.

One more question please, about power estimator.

Is there power estimator tool that can help me estimate how much power the IMX consume when I'm using both CSI-2 inputs (with the internal ISP and compress block 265/264) and general IO's ?

0 件の賞賛
返信

9,082件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Yoav Benita,

We do not have a document with that measure in specific but, we have the i.MX 8M Plus Evaluation Kit enabling Power Measurement that has Board Remote Control Utilities(BCU), this allows you to measure different power rails.

As a reference the MIPI's power rails has a max current consumption of:

VDD_MIPI_0V8: 100 mA
VDD_MIPI_1V8: 50 mA

You can check it on i.MX 8M Plus Power Measurement Board User's Guide, I will attach the file on this answer.

Best regards.

0 件の賞賛
返信

9,065件の閲覧回数
YoavBenita
Contributor II

Hi 

Thank you