IMX8MP use ISI with ISP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP use ISI with ISP

10,970 Views
quercuspau
Contributor II

Hello community,

I have connected a RAW10 camera to ISP from IMX8MP. My question is if it is possible to connect the output stream of the ISP to ISI to transform the YUV image to RGB format.

Looking at the TRM, i am not sure if it is possible.

BR

0 Kudos
Reply
14 Replies

9,337 Views
Saravanans1
Contributor III

Hi,

Will it support IMX8MPlus for RAW16 format ?. If it is supporting can you send me the reference designs or documents ?

0 Kudos
Reply

10,641 Views
malik_cisse
Senior Contributor I

Hi Quercuspau,

Could you actually succeed capturing RGB?

I found your suggestion to read AXI interesting. Would be great if we can do that.
For snapshots I am using Bayer RG12 raw images that I convert to RGB using software ISP. This is not practical for live video tough,

BR

0 Kudos
Reply

10,614 Views
quercuspau
Contributor II

Hi Malik,

Yes, it is possible. Do you need to enable M2M device tree node from ISI0 in device tree. Then you will be able to use v4l2convert element from gstreamer to transform YUV to RGB for instance:

gst-launch-1.0 v4l2src device=/dev/video2 num-buffers=1 io-mode=dmabuf ! video/x-raw, width=1920, height=1080 ! v4l2convert output-io-mode=dmabuf-import ! video/x-raw, width=1920, height=1080, format=RGB ! filesink location=image_1080p_RGB888.rgb

BR

0 Kudos
Reply

10,597 Views
malik_cisse
Senior Contributor I

Thank you for the feedback,

YUV 4:2:2 is already downsampled. When converting YUV back to RGB, one will not get original resolution. Missing pixels are computed. The idea is to get best possible quality after ISP.

In my case, the sensor (imx477) is actually providing 4056x3040 pixels at 12bpp. After ISP treatment only 8bit YUYV will be left.

After de-mosaicing, the ISP has 12Bit RGB internally as can be seen in ISP pipeline flow chart, however this HDR picture is down-converted to YUYV (yuv 4:2:2) prior to write AXI bus.

The question is how to get higher bit-depth ISP processed image? The intermediate ISP steps must be somewhere in the memory. Ideally I am interested in 12bpp RGB or at least 8bit RGB.

BR, MC

 

 

0 Kudos
Reply

10,593 Views
quercuspau
Contributor II

Maybe some employee from NXP can answer your last question. But my assumption is: being the ISP a closed peripheral and having its own static RAM. I dont think that you can get the data from the intermediate steps of the ISP. So you will be forced the do the debayern from output RAWs using SoftISP.

BR

10,938 Views
joanxie
NXP TechSupport
NXP TechSupport

you can use ISP directly, don't need to use ISI, you can refer to the dts file, which support basler camera via ISP

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-b..."

 

0 Kudos
Reply

10,928 Views
quercuspau
Contributor II

ISP only provides YUV or RAW. ISI is able to deliver RGB. I would like to use both ISI channels connected to one ISP stream to get different format RGB video streams

BR

0 Kudos
Reply

10,923 Views
joanxie
NXP TechSupport
NXP TechSupport

one can use GPU to convert YUV to RGB

 

0 Kudos
Reply

10,921 Views
quercuspau
Contributor II

Is it not possible to do it with ISI?

BR

0 Kudos
Reply

10,878 Views
joanxie
NXP TechSupport
NXP TechSupport

ISI is supposed to connect to mipi csi2 interface, pls see the pic as below:

joanxie_1-1638177046963.png

 

joanxie_0-1638176985459.png

 

 

0 Kudos
Reply

10,865 Views
quercuspau
Contributor II

Hello @joanxie ,

I just found this information on TRM:

ISI_memory_read.png

However, I haven't found any document about how to use this functionality with NXP Linux BSP.

Could you provide this information?

BR

0 Kudos
Reply

10,858 Views
joanxie
NXP TechSupport
NXP TechSupport

ISI supports isi.m2m device and isi.cap device, you can test by ov5640, you can refer to the dts file:

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk.d...

isi_0{

status = "okay";

cap_device {

status = "okay";

};

m2m_device {

status = "okay";

};

};

&isi_1 {

status = "disabled";

cap_device {

status = "okay";

};

they both connect to the camera, for isi source code, one can refer to:

"https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx/imx8-isi-m2m.c?h..."

 

0 Kudos
Reply

10,851 Views
quercuspau
Contributor II

Is there no more information?

BR

0 Kudos
Reply

10,841 Views
joanxie
NXP TechSupport
NXP TechSupport

I explain again, Memory can be the source of ISI, but current bsp doesn't support this, and I consult local team, no one did this and no sample for this, maybe you need to ask for professional support for your special demands

"https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and..."

0 Kudos
Reply