IMX8MP take a long time to enter sleep ( RAM retention mode )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP take a long time to enter sleep ( RAM retention mode )

1,124 Views
cduarte0306
Contributor II

Hi all,

I am working with an IMX8MP using Kernel version 6.1.1.

I have noticed a rather annoying issue when trying to place the unit to sleep via the following command: 

 

 

 

echo mem > /sys/power/state"

 

 

 

 

After initial boot, this command takes anywhere from 10 to 30 seconds to take place and actually place the unit in low power mode. In the meantime, it is able to respond to terminal commands and perform other actions. 

I should note this only ever happens once until power-cycled. In any other case, the CPU enters sleep mode instantaneously. This only happens after initial boot. Has anyone else had this issue?

 

Thanks

Carlos

Tags (2)
0 Kudos
Reply
4 Replies

754 Views
PunitTeksun
Contributor I

Hello,

Does this RAM retention mode also supported in the Android OS on IMX8MP evk ?

0 Kudos
Reply

1,091 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @cduarte0306

Thank you for contacting NXP Support.

I have tested the issue on our i.MX8M Plus EVK and it is working fine.
Are you using a custom board?

Have a great day!

0 Kudos
Reply

1,088 Views
cduarte0306
Contributor II

I am using a SOM by Karo Electronics with Kernel version 6.1.1.

 

Did you it as soon as it was power cycled?

0 Kudos
Reply

1,064 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @cduarte0306

Yes, I tested in that situation.

I suggest you review the i.MX Linux Reference Manual section 2.5 Power Management to check a possible misconfiguration in your custom board.

I hope this information will be helpful.

Have a great day!

0 Kudos
Reply