[IMX8MP ISP] RAW RGB-IR sensor support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[IMX8MP ISP] RAW RGB-IR sensor support

Jump to solution
5,761 Views
khang_letruong
Senior Contributor III

Dear Community,

I would like to know if the ISP inside IMX8MP supports demosiacing RAW RGB-IR sensors which seem to have different pattern of Color Filter Array (CFA) compared to RAW Bayer, please ?

Standard Bayer Pattern :

Figure-1-Bayer-pattern-05-300x269.jpg

RGB-IR filter pattern :

Figure-2-RGB-IR-filter-pattern-08-300x269.jpg

Thanks in advance and best regards,
Khang

Tags (1)
1 Solution
5,672 Views
dianapredescu
NXP Employee
NXP Employee

@khang_letruong,

I received confirmation. "Yes, this is a HW limitation, 8mp ISP doesn’t support RGB-IR. It can only support Bayer RGB or Monochrome." 

Best regards,

Diana

View solution in original post

0 Kudos
Reply
9 Replies
5,709 Views
dianapredescu
NXP Employee
NXP Employee

Hi Khang,

If I remember correctly, some time ago there were some discussions on this topic and the conclusion was that "8MP ISP only support Bayer RGB". 

Regards,

Diana

0 Kudos
Reply
5,706 Views
khang_letruong
Senior Contributor III

Hi @dianapredescu ,

Could you give me the link(s) of those discussions if possible, please ?

Best Regards,

K.

 

 

0 Kudos
Reply
5,689 Views
khang_letruong
Senior Contributor III

Hi @dianapredescu ,

Could you share the discussions that you mentioned, please ?

 

Thanks in advance and best regards,
K.

0 Kudos
Reply
5,681 Views
dianapredescu
NXP Employee
NXP Employee

Hi Khang,

so sorry for missing the first reply. Unfortunately there was an internal discussion and I don't have any links as reference. But let me check once again with R&D and I'll get back to you today.

Best regards,

Diana

5,673 Views
dianapredescu
NXP Employee
NXP Employee

@khang_letruong,

I received confirmation. "Yes, this is a HW limitation, 8mp ISP doesn’t support RGB-IR. It can only support Bayer RGB or Monochrome." 

Best regards,

Diana

0 Kudos
Reply
3,456 Views
splatspeed1
Contributor I

hi diana @dianapredescu 

if we correct the bayer pattern in SW can we use the ISP as memory to memory. or as i believe is it only available as camera sensor to memory. i.e. can we use memory as an interface to the ISP or is it rigidly locked to the HW.

 

thx in advance Sean

0 Kudos
Reply
5,662 Views
khang_letruong
Senior Contributor III

HI @dianapredescu ,

Thanks a lot for your confirmation.

Best Regards,
K.

0 Kudos
Reply
5,742 Views
khang_letruong
Senior Contributor III

Hi Again,

From the Reference Manual of iMX 8M Plus, it seems that RGB-IR is not in the list of supported input formats :

ISP_INPUTs.png

 

Could someone confirm, please ?

Best Regards,
K.

 

0 Kudos
Reply
5,717 Views
khang_letruong
Senior Contributor III

Dear @joanxie,

Could you help to escalate this question to internal team for confirmation, please ?

Thanks in advance and best regards,
Khang

 

0 Kudos
Reply