IMX8MP: How to mirror two screens on dual display(HDMI+LVDS or Mipi)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MP: How to mirror two screens on dual display(HDMI+LVDS or Mipi)

2,603 次查看
KrisLan
Contributor II

My device connects to two screens(HDMI+LVDS or Mipi),with the same resolution 1920x1080. I need two screens display the same, mirrored content.

Is there any soultions to support it? If the SOCs(IMX8M Plus or IMX8M Quad) doesn't support this application, is there other SOCs which can support it?

OS:Android 11

SOC: IMX8M Plus or IMX8M Quad

 

0 项奖励
回复
5 回复数

1,329 次查看
navya_dixit
Contributor V

Is there any update on this? We are also having same requirement: i.MX8MP with display mirroring support. Is it possible with i.MX8MP?

0 项奖励
回复

1,324 次查看
KrisLan
Contributor II

We did not use IMX8MP and copy hdmi output signal directly.

2,588 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @KrisLan 

I.MX8QM supports  multiple displays in default BSP

0 项奖励
回复

2,577 次查看
KrisLan
Contributor II

I checked the NXP website just now.  I.MX8QM is I.MX8 Quad Max?

It support multiple displays  by using its "

  • 2x Display Processor Controllers with inline blending and WARP" ?

 

标记 (1)
0 项奖励
回复

2,584 次查看
KrisLan
Contributor II

Qmiller, thanks for your time!

"I.MX8QM" is i.MX 8M Quad ? Does the multiple displays you mentioned supports Duplicate Mode or Extend Mode or both two modes in default BSP of Android OS?

If I prefer to use i.MX 8M Plus, Android OS, I need to release this application by myself for the default BSP doesn't support in IMX8MP?

0 项奖励
回复