[IMX8MP] Debug OpenCL using VivanteIDE5.4 on hardware does NOT hit breakpoint in OpenCL kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[IMX8MP] Debug OpenCL using VivanteIDE5.4 on hardware does NOT hit breakpoint in OpenCL kernel

1,288件の閲覧回数
dteng
Contributor I

I'm trying to debug OpenCL kernel using VivanteIDE5.4. The board is running Yocto BSP version 5.15.5 recently released. I was able to setup the IDE so that the sample project - cl_multi_context can be built successfully and was able to launch debug so that the problem breaks at the main function. My issue was that the program will never go into the OpenCL during debug single stepping.

The things I've tried:

  • Turns on "Generate debug information (-g) in the "Cross OpenCL Compiler" setting, following the steps in the Vivante_IDE_User_guide.pdf
  • Set Default work-item for new breakpoints to be 0,0,0

Screenshot from 2022-05-19 13-10-08.pngScreenshot from 2022-05-19 13-10-08.png

After doing all these, the program still simply doesn't go into the kernel while debugging. In fact, I wasn't able to set breakpoint in the kernel source code (mathop.cl). When I examine the vdb item on left, it doesn't include any Context items which is showing in the images included in the Vivante_IDE_User_guide.pdf

Anyone has any idea what's going on?

0 件の賞賛
返信
0 返答(返信)