IMX8MP CAN FD test failed at a data bitrate of 6000k.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MP CAN FD test failed at a data bitrate of 6000k.

跳至解决方案
2,981 次查看
charleshuang
Senior Contributor II

Hi NXP Team

Our customer tested CAN bus FD, and the test failed.

They tried setting the data bitrate to 6000k, but it failed.

However, setting the data bitrate to 5000k passed.

Do you have any advice?

Test command:  (Test 6000k Fail.)

ip link set can0 up type can bitrate 1000000 dbitrate 6000000  fd on

ip link set can1 up type can bitrate 1000000 dbitrate 6000000  fd on

charleshuang_0-1723018914421.jpeg

 

Test 5000k pass.

charleshuang_1-1723018978676.jpeg

标签 (1)
0 项奖励
回复
1 解答
2,907 次查看
kef2
Senior Contributor V
Your customer shouldn't ignore "bitrate error 4,7%" message. As you see, he doesn't have such error with 5Mbps.
You can't use every bit rate you wish, but only those, which your CAN clock allows. You didn't specify what is your CAN clock. With 80MHz 8, 5, 4, 3.2, 2.5, 1.6, 1Mbps are possible plus those below 1Mbps. With 40MHz 3.2 is not possible, perhaps 1.6 as well, must check. For 6Mbps I guess you need 30 or 60MHz clock, try calculating it yourself.

在原帖中查看解决方案

6 回复数
2,908 次查看
kef2
Senior Contributor V
Your customer shouldn't ignore "bitrate error 4,7%" message. As you see, he doesn't have such error with 5Mbps.
You can't use every bit rate you wish, but only those, which your CAN clock allows. You didn't specify what is your CAN clock. With 80MHz 8, 5, 4, 3.2, 2.5, 1.6, 1Mbps are possible plus those below 1Mbps. With 40MHz 3.2 is not possible, perhaps 1.6 as well, must check. For 6Mbps I guess you need 30 or 60MHz clock, try calculating it yourself.
2,879 次查看
charleshuang
Senior Contributor II

Hi  @kef2 

We followed the NXP i.MX8MP DTSI settings, where the CAN clock is set to 40 MHz.

Do you know what the maximum bitrate value could be test pass?

Thanks.

0 项奖励
回复
2,875 次查看
kef2
Senior Contributor V

Hi,

I think I wrote already, @40MHz CAN clock, 8Mbps is achievable. The most close speeds are 5 and 8Mbps, no more speeds in between @40Mhz.

Please don't forget as well capabilities of transceiver chips, you are using. 

0 项奖励
回复
2,831 次查看
charleshuang
Senior Contributor II

@kef2 

Thanks about your help.  8Mbps pass.

0 项奖励
回复
2,942 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? Are you using NXP evk board or the board you design youself?

0 项奖励
回复
2,910 次查看
charleshuang
Senior Contributor II

@Rita_Wang 

About our Image OS is Yocto 3.0-5.4.70.

0 项奖励
回复