I am working on an uplift from kirkstone (uboot-imx 2022.04) to scarthgap using IMX BSP.
System is custom based on the IMX8MN with LPDDR4.
The commit in branch of uboot-imx which is based on:
commit de16f4f17221b2ff72b8cb18c28cd8a29f3c2710 (HEAD -> lf_v2024.04, tag: lf-6.6.36-2.1.0, tag: android-14.0.0_2.2.0, origin/lf_v2024.04)
Trying to start SPL for flashing via uuu gives.
3:3>Start Cmd:SDPS: boot -f >/nix/store/dljgvki41iynrwc2l5an6l99v5pnzx2g-sign-all-the-things/flash.bin
15%3:3>Fail HID(W):LIBUSB_ERROR_TIMEOUT(1.045s)
And reading the uart output says:
U-Boot SPL 2024.04-imx_v2024.04_6.6.36-2.1.0+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000)
Failed to find clock node. Check device tree
Adding some more debug to u-boot gives additional information:
clock-controller@30380000: could not find phandle, phandle: 20, cur_index: 0
clk_get_by_index_tail: Node 'clock-controller@30380000', property 'clocks', failed to request CLK index 1: -22
Failed to find clock node. Check device tree
The probe of fsl,imx8mn-ccm fails when trying to find osc_24m in DTB.
Code (clk-imx8mn.c)
ret = clk_get_by_name(dev, "osc_24m", &osc_24m_clk);
if (ret) {
return ret;
}
Code: (fdtdec.c)
if (cells_name || cur_index == index) {
node = fdt_node_offset_by_phandle(blob, phandle);
if (node < 0) {
printf("%s: could not find phandle, phandle: %d, cur_index: %d\n",
fdt_get_name(blob, src_node, NULL), phandle, cur_index);
goto err;
}
}
So if I modify clk-uclass.c to not use cell_name, #clock-cells,
it will proceed a bit further but fail at other points. This is obviously not the way forward but perhaps can shed some light at whats wrong?
clk_get_by_index_nodev(ofnode node, int index, struct clk *clk)
{
struct ofnode_phandle_args args;
int ret;
ret = ofnode_parse_phandle_with_args(node, "clocks", "#clock-cells", 0,
index, &args);
The DTS code adjacent to the error is as follows:
imx8mn.dtsi:
clk: clock-controller@30380000 {
compatible = "fsl,imx8mn-ccm";
reg = <0x30380000 0x10000>;
#clock-cells = <1>;
clocks = <&osc_32k>, <&osc_24m>, <&clk_ext1>, <&clk_ext2>,
<&clk_ext3>, <&clk_ext4>;
clock-names = "osc_32k", "osc_24m", "clk_ext1", "clk_ext2",
"clk_ext3", "clk_ext4";
assigned-clocks = <&clk IMX8MN_CLK_A53_SRC>,
<&clk IMX8MN_CLK_A53_CORE>,
<&clk IMX8MN_CLK_NOC>,
<&clk IMX8MN_CLK_AUDIO_AHB>,
<&clk IMX8MN_CLK_IPG_AUDIO_ROOT>,
<&clk IMX8MN_SYS_PLL3>,
<&clk IMX8MN_VIDEO_PLL1>,
<&clk IMX8MN_AUDIO_PLL1>,
<&clk IMX8MN_AUDIO_PLL2>;
assigned-clock-parents = <&clk IMX8MN_SYS_PLL1_800M>,
<&clk IMX8MN_ARM_PLL_OUT>,
<&clk IMX8MN_SYS_PLL3_OUT>,
<&clk IMX8MN_SYS_PLL1_800M>;
assigned-clock-rates = <0>, <0>, <0>,
<400000000>,
<400000000>,
<600000000>,
<1039500000>,
<393216000>,
<361267200>;
};
From custom device tree usage of the same node via phandle:
&clk {
bootph-pre-ram;
bootph-all;
/delete-property/ assigned-clocks;
/delete-property/ assigned-clock-parents;
/delete-property/ assigned-clock-rates;
};
&osc_24m {
bootph-pre-ram;
bootph-all;
};
Something is obviously missing in this migration.
I am attaching the DTS sources.
What is the problem?
Is there some official migration guide to follow 2022->2024?
Thanks!
Solved! Go to Solution.
Hello,
Could you share how you are creating/building your boot image?
Also, from where are you getting the source code?
Best regards/Saludos,
Aldo.