IMX8MN pinfunc typo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MN pinfunc typo

Jump to solution
552 Views
BartholomeusDias
Contributor I

Hi,

I'm not sure if this is the right place to post, but I think I have found a typo in imx8mn-pinfunc.h

diff --git a/arch/arm64/boot/dts/freescale/imx8mn-pinfunc.h b/arch/arm64/boot/dts/freescale/imx8mn-pinfunc.h
index faf1e69e742b..2288b16bb48b 100644
--- a/arch/arm64/boot/dts/freescale/imx8mn-pinfunc.h
+++ b/arch/arm64/boot/dts/freescale/imx8mn-pinfunc.h
@@ -474,7 +474,7 @@
 #define MX8MN_IOMUXC_SAI3_RXD_UART2_DCE_RTS_B     0x1D4 0x43C 0x4F8 0x4 0x3
 #define MX8MN_IOMUXC_SAI3_RXD_UART2_DTE_CTS_B     0x1D4 0x43C 0x000 0x4 0x0
 #define MX8MN_IOMUXC_SAI3_RXD_GPIO4_IO30          0x1D4 0x43C 0x000 0x5 0x0
-#define MX8MN_IOMUXC_SAI3_RXD_PDM_BIT_STREAM1     0x1D4 0x43C 0x538 0x6 0x10
+#define MX8MN_IOMUXC_SAI3_RXD_PDM_BIT_STREAM1     0x1D4 0x43C 0x538 0x6 0xA
 #define MX8MN_IOMUXC_SAI3_TXFS_SAI3_TX_SYNC       0x1D8 0x440 0x000 0x0 0x0
 #define MX8MN_IOMUXC_SAI3_TXFS_GPT1_CAPTURE2      0x1D8 0x440 0x5EC 0x1 0x0
 #define MX8MN_IOMUXC_SAI3_TXFS_SAI5_RX_DATA1      0x1D8 0x440 0x4D8 0x2 0x1


I have spent the last two days trying to figure out why on earth my pdm microphone would not work, but now it does.

Hope it will find it's way!

Labels (1)
0 Kudos
Reply
1 Solution
528 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @BartholomeusDias ,

I hope you're doing great! I've let our team know, thank you.

Best regards,
Hector.

View solution in original post

1 Reply
529 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @BartholomeusDias ,

I hope you're doing great! I've let our team know, thank you.

Best regards,
Hector.