IMX8MN USB OTG not recognized (when doing ddr test)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MN USB OTG not recognized (when doing ddr test)

ソリューションへジャンプ
2,209件の閲覧回数
AccuJie
Contributor III

Hi

We have three customized IMX8MN boards. Now, we are trying to do the ddr training & stress test.

However, two of our boards are not recognized by the PC at all. Another one just got a warning of USB device not recognized. We already changed the boot mode to serial download mode.

AccuJie_0-1637092330741.png

 

Of cause we got the error inside ddr training and stress test tools:

ERROR: Can't open USB device!!!
Please check if the correct target is selected and set to the serial download mode

 

We are using the PMIC of PCA9450 with a 2Gb DDR4. Here is the power rail supply from the pmic I measured(when in serial download mode before firmware download):

VSYS_5V5V
PCA9450B_BUCK1(VDD_SOC&VDD_DRAM)0.85V
PCA9450B_BUCK2(VDD_ARM)0.85V
PCA9450B_BUCK4(VDD_3V3/NVCC_3V3)3.3V
PCA9450B_BUCK5(VDD_1v8/NVCC_1V8)1.8V
PCA9450B_BUCK6(NVCC_DRAM)1.1V
PCA9450B_LDO1(NVCC_SNVS_1V8)1.78V
PCA9450B_LDO2(VDD_SNVS_0V8 )0.8V
PCA9450B_LDO3(1V8_VDDA)1.8V

Base on my understanding, the firmware download in ddr test tools(download into on-chip internal RAM) only needs the basic voltage(default config).

Where should I have a check in the next step?

Thanks.

0 件の賞賛
返信
1 解決策
2,202件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jie

 

for that issue one can check sect.Table 8. USB recommendations, clock stability

using sect.Table 10. Oscillator/Crystal recommendations     i.MX 8M Nano Hardware Developer’s Guide

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,203件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jie

 

for that issue one can check sect.Table 8. USB recommendations, clock stability

using sect.Table 10. Oscillator/Crystal recommendations     i.MX 8M Nano Hardware Developer’s Guide

 

Best regards
igor

0 件の賞賛
返信
2,183件の閲覧回数
AccuJie
Contributor III

Thanks for your suggestion. We found out that the problem is from our oscillator. 

0 件の賞賛
返信