IMX8MM raydium panel setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM raydium panel setup

1,763件の閲覧回数
ppavacic
Contributor II

Hello,

IMX Linux Integration manual doesn't quite explain MIPI DSI Panel integration.

Lets start with device tree:

https://github.com/varigit/linux-imx/blob/5.15-2.0.x-imx_var01/arch/arm64/boot/dts/freescale/imx8mm-... show us that in order to add panel we should just add panel to the &mipi_dsi device tree.

While https://github.com/varigit/linux-imx/blob/5.15-2.0.x-imx_var01/Documentation/devicetree/bindings/dis...

shows us that mipi-dsi requires two ports to be defined and second port should be connected to the MIPI display.

That goes well with the documentation for raydium device tree which can be found here:

https://www.kernel.org/doc/Documentation/devicetree/bindings/display/panel/raydium%2Crm67191.yaml

Therefore final device tree according to my logic should look something like this:

&lcdif {
	status = "okay";
};

&mipi_dsi {
	status = "okay";
	
	panel@0 {
		status = "okay";
		reg = <0>;
		compatible = "raydium,rm67191"; 
		dsi-lanes = <2>;
		pinctrl-names = "default";
		reset-gpios = <&gpio1 11 GPIO_ACTIVE_HIGH>;
		width-mm = <56>;
		height-mm = <93>;
		//video-mode = <2>;
		
		port {
			panel_in: endpoint {
				remote-endpoint = <&mipi_out>;
			};
		};
	};
	
	port@0 {
		dsim_from_lcdif: endpoint {
			remote-endpoint = <&lcdif_to_dsim>;
		};
	};
	
	port@1 {
		mipi_out: endpoint {
        	remote-endpoint = <&panel_in>;
  		};
	};
};

 

Can you please clarify how it should be done.

0 件の賞賛
返信
1 返信

1,749件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You just need to replacement the dtb of general community by the NXP one and see if one of the GPIO is not used.

regards

0 件の賞賛
返信