IMX8MM mini UUU without type C connector

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MM mini UUU without type C connector

2,139 次查看
dudisasson
Contributor I

Hi,

I have a new board we designed according to the IMX8MM mini EVK. we removed the type C connectors and replaced them with an usb2 OTG connectors. 

I used the following link and compiled the Uboot & kernel with the changes mentioned there.

 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-US...

Uboot - CONFIG_USB_TCPC=n

Device tree - 

&usbotg1 {
    status = "okay";
};

&usbotg2 {
    status = "okay";

and removed the references to ptn5110.

when trying to load them with UUU, this is what I get in the terminal:

U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Feb 11 2021 - 14:16:20 +0000)
power_bd71837_init
DDRINFO: start lpddr4 ddr init
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from USB SDP
SDP: initialize...
SDP: handle requests...
Downloading file of size 1223624 to 0x40400000... done
Jumping to header at 0x40400000
Header Tag is not an IMX image
Found header at 0x4042b400


U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Feb 11 2021 - 14:16:20 +0000)

CPU:   Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 35C
Reset cause: POR
Model: FSL i.MX8MM EVK board
DRAM:  2 GiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Card did not respond to voltage select!
*** Warning - No block device, using default environment

Failed (-5)
No panel detected: default to MIPI2HDMI
adv7535_init: Can't find device id=0x3d, on bus 1
Display: MIPI2HDMI (1920x1080)
Video: 1920x1080x24
In:    serial
Out:   serial
Err:   serial

 BuildInfo:
  - ATF 1cb68fa
  - U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df

Card did not respond to voltage select!
Detect USB boot. Will enter fastboot mode!
Net:   No ethernet found.
Fastboot: Normal
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot:  0

## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
g_dnl_register: failed!, error: -19
u-boot=>



Any ideas?

Thanks in advance,
Dudi/

 

 

 

0 项奖励
回复
3 回复数

1,697 次查看
maidaothanh
Contributor I

could you plwase share me the BIN file

0 项奖励
回复

2,086 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi dudisasson,

 

It appear that all the configuration you did is good, where did you take the source code?

 

Regards,

Israel H.

0 项奖励
回复

2,071 次查看
dudisasson
Contributor I

Hi Israel,

the source code is from the following link:

https://source.codeaurora.org/external/imx/imx-manifest 

I am using imx-linux-sumo

 

 

 

0 项奖励
回复