IMX8MM evakit (8MMINILPD4-EVK) doesn't boot out of the box

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM evakit (8MMINILPD4-EVK) doesn't boot out of the box

3,063 Views
kariviit
Contributor I

Hi,

I received  this week two 8MMINILPD4-EVK kits and both of them are not booting to Android out of the box. According to serial terminal they tried to start Android, but booting fails and board reboots itself after a while. I also downloaded a new Android image (android_p9.0.0_1.0.0-ga_image_8mmevk.tar.gz) and I downloaded it to the board using serial download tool. It behaves a similar way and it didn't boot either. 

There seems to be a problem with this pre-built Android image. 

Maybe someone could help me and others?

 

BR Kari,

 

Captured bootlog is following: 

U-Boot SPL 2018.03 (Dec 19 2018 - 17:39:10 +0800)
power_bd71837_init
DDRINFO: start lpddr4 ddr init
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC2


U-Boot 2018.03 (Dec 19 2018 - 17:39:10 +0800)

CPU: Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 55C
Reset cause: POR
Model: FSL i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF d6451cc
- U-Boot 2018.03

flash target is MMC:1
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
verify OK, boot 'boot_a'
Kernel load addr 0x40480000 size 30737 KiB
kernel @ 40480000 (31474176)
ramdisk @ 43600000 (7425471)
fdt @ 43400000 (43646)
## Flattened Device Tree blob at 43400000
Booting using the fdt blob at 0x43400000
Using Device Tree in place at 0000000043400000, end 000000004340da7d

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.78 (bamboo@szandroidmpu-PowerEdge-T430) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #1 SMP PREEMPT Wed Dec 19 17:42:18 CST 2018
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: FSL i.MX8MM EVK board
[ 0.000000] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[ 0.000000] bootconsole [ec_imx6q0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 800 MiB at 0x0000000086000000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbffbc900-0xbffbe6ff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] random: get_random_bytes called from start_kernel+0xa8/0x414 with crng_init=0
[ 0.000000] percpu: Embedded 25 pages/cpu @ffff80007ff52000 s64792 r8192 d29416 u102400
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 515072
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init androidboot.console=ttymxc1 androidboot.hardware=freescale cma=800M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware transparent_hugepage=never buildvariant=userdebug androidboot.serialno=2b13320a5c85d94a androidboot.btmacaddr=2b:13:32:0a:5c:85 androidboot.soc_type=imx8mm androidboot.storage_type=emmc androidboot.boottime=1BLL:0,1BLE:5010,KL:0,KD:0,AVB:1690,ODT:0,SW:0 androidboot.bootreason=cold,powerkey androidboot.verifiedbootstate=green androidboot.slot_suffix=_a dm="1 vroot none ro 1,0 3611944 verity 1 PARTUUID=009c6079-5025-4c43-8f12-8ceec8aac5ab PARTUUID=009c6079-5025-4c43-8f12-8ceec8aac5ab 4096 4096 451493 451493 sha1 205d7577d21244e9aac3254b1de644a3a5646c68 ab818cfd25b335452dfcb11bc8373316a419746c 10 restart_on_corruption ignore_zero_blocks use_fec_from_device PARTUUID=009c6079-5025-4c43-8f12-8ceec8aac5ab fec_roots 2 fec_blocks 455050 fec_start 455050" r
[ 0.000000] device-mapper: init: will configure 1 devices
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Memory: 1209012K/2093056K available (15804K kernel code, 2384K rwdata, 7008K rodata, 5504K init, 534K bss, 64844K reserved, 819200K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000
[ 4.400151] audit: type=1400 audit(1545213107.196:4): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 4.404257] ueventd: ueventd started!
[ 4.407762] selinux: SELinux: Loaded file_contexts
[ 4.407762]
[ 4.408087] ueventd: Parsing file /ueventd.rc...
[ 4.410684] ueventd: Parsing file /vendor/ueventd.rc...
[ 4.411374] ueventd: Parsing file /odm/ueventd.rc...
[ 4.411411] ueventd: Unable to read config file '/odm/ueventd.rc': open() failed: No such file or directory
[ 4.411774] ueventd: Parsing file /ueventd.freescale.rc...
[ 4.411799] ueventd: Unable to read config file '/ueventd.freescale.rc': open() failed: No such file or directory
[ 4.468718] audit: type=1400 audit(1545213107.196:5): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 4.472101] ueventd: firmware: loading 'imx/sdma/sdma-imx7d.bin' for '/devices/platform/30bd0000.dma-controller/firmware/imx!sdma!sdma-imx7d.bin'
[ 4.475252] ueventd: loading /devices/platform/30bd0000.dma-controller/firmware/imx!sdma!sdma-imx7d.bin took 3ms
[ 4.510418] audit: type=1400 audit(1545213107.196:6): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 4.528282] audit: type=1400 audit(1545213107.196:7): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 4.546311] audit: type=1400 audit(1545213107.200:8): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 4.546794] imx-sdma 302c0000.dma-controller: loaded firmware 4.4
[ 4.565009] imx-sdma 302b0000.dma-controller: loaded firmware 4.4
[ 4.566060] imx-sdma 30bd0000.dma-controller: loaded firmware 4.4
[ 4.582504] audit: type=1400 audit(1545213107.200:9): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 4.600094] audit: type=1400 audit(1545213107.200:10): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 4.625329] Registered swp emulation handler
[ 4.635128] watchdogd: watchdogd started (interval 10, margin 20)!
[ 4.642136] Console: switching to colour dummy device 80x25
[ 4.660750] EXT4-fs (mmcblk2p12): Ignoring removed nomblk_io_submit option
[ 4.690019] wlan: loading driver v4.5.23.1
[ 4.696498] hifDeviceInserted: Dumping clocks (50000000,400000000)
[ 4.702758] AR6000: Set async interrupt delay clock as 2.
[ 4.811643] EXT4-fs (mmcblk2p12): recovery complete
[ 4.817080] EXT4-fs (mmcblk2p12): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
[ 4.833590] AR6000: configuration opcode 3 is not used for Linux SDIO stack
[ 4.841263] NUM_DEV=1 FWMODE=0x2 FWSUBMODE=0x0 FWBR_BUF 0
[ 5.207943] random: crng init done
[ 5.246200] HIF Interrupt processing is SYNC ONLY
[ 5.250935] AR6000: configuration opcode 7 is only used for RTOS systems, not Linux systems
[ 5.259314] AR6000: configuration opcode 5 is not used for Linux SDIO stack
[ 5.267174] +HWT
[ 5.274685] -HWT
[ 5.276658] MAILBOX SWAP Service is enabled!
[ 5.280966] Reduced Tx Complete service is enabled!
[ 5.287195] HTCConnectService, host indicate support b2b bundle
[ 5.294394] HTCConnectService, firmware decide to disabled b2b bundle
[ 5.300877] HTC Service:0x0300 ep:1 TX flow control disabled
[ 5.307219] HTCConnectService, host indicate support b2b bundle
[ 5.313391] HTCConnectService, firmware decide to disabled b2b bundle
[ 5.336565] target uses HTT version 3.51; host uses 3.28
[ 5.355999] Host SW:4.5.23.1, FW:0.0.0.27, HW:QCA93x7_REV1_1
[ 5.362280] ol_pktlog_init: pktlogmod_init successfull
[ 5.368799] ath_hif_sdio: HIF (Atheros/multi-bss)
[ 5.373608] wlan: driver loaded in 684000
[ 5.899060] e2fsck: e2fsck 1.43.3 (04-Sep-2016)
[ 5.899060]
[ 5.905172] e2fsck: Pass 1: Checking inodes, blocks, and sizes
[ 5.905172]
[ 5.912534] e2fsck: Pass 2: Checking directory structure
[ 5.912534]
[ 5.919381] e2fsck: Pass 3: Checking directory connectivity
[ 5.919381]
[ 5.926450] e2fsck: Pass 4: Checking reference counts
[ 5.926450]
[ 5.933004] e2fsck: Pass 5: Checking group summary information
[ 5.933004]
[ 5.940333] e2fsck:
[ 5.940333]
[ 5.944023] e2fsck: /dev/block/by-name/userdata: ***** FILE SYSTEM WAS MODIFIED *****
[ 5.944023]
[ 5.953351] e2fsck: /dev/block/by-name/userdata: 1459/581632 files (2.7% non-contiguous), 71133/2326528 blocks
[ 5.953351]
[ 5.970256] EXT4-fs (mmcblk2p12): Ignoring removed nomblk_io_submit option
[ 5.984110] EXT4-fs (mmcblk2p12): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
[ 6.027852] zram0: detected capacity change from 0 to 314572800
[ 6.055497] logd.auditd: start
[ 6.058548] mkswap: Swapspace size: 307196k, UUID=4597bba0-4899-4f69-a859-01cb82b0bdce
[ 6.066720] logd.klogd: 5919249125
[ 6.067600] Adding 307196k swap on /dev/block/zram0. Priority:-2 extents:1 across:307196k SS
[ 6.111712] type=1400 audit(1545213108.868:38): avc: denied { getattr } for pid=2470 comm="init" path="/data/cache" dev="mmcblk2p12" ino=262159 scontext=u:r:vendor_init:s0 tcontext=u:object_r:cache_file:s0 tclass=dir permissive=0
[ 6.132714] type=1400 audit(1545213108.868:38): avc: denied { getattr } for pid=2470 comm="init" path="/data/cache" dev="mmcblk2p12" ino=262159 scontext=u:r:vendor_init:s0 tcontext=u:object_r:cache_file:s0 tclass=dir permissive=0
[ 6.153263] type=1400 audit(1545213108.868:39): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[ 6.401585] update_verifier: Started with arg 1: nonencrypted
[ 6.410914] update_verifier: Booting slot 0: isSlotMarkedSuccessful=1
[ 6.417446] update_verifier: Leaving update_verifier.
[ 6.456999] rfkill: BT RF going to : off
[ 6.462590] logd.daemon: reinit
[ 6.486862] Mass Storage Function, version: 2009/09/11
[ 6.492039] LUN: removable file: (no medium)
[ 6.499759] using random self ethernet address
[ 6.504266] using random host ethernet address
[ 6.510623] file system registered
[ 6.633355] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 6.800728] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
evk_8mm:/ $ [ 7.106743] audit_log_lost: 29 callbacks suppressed
[ 7.106750] audit: audit_lost=494 audit_rate_limit=5 audit_backlog_limit=64
[ 7.147630] audit: rate limit exceeded
[ 7.284788] read descriptors
[ 7.299574] read strings
[ 8.625832] capability: warning: `main' uses 32-bit capabilities (legacy support in use)
[ 11.086668] type=1400 audit(1545213111.616:577): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0 duplicate messages suppressed
[ 11.092509] audit: audit_lost=523 audit_rate_limit=5 audit_backlog_limit=64
[ 11.092511] audit: rate limit exceeded
[ 11.117391] type=1400 audit(1545213113.880:578): avc: denied { dac_read_search } for pid=3164 comm="Binder:3164_1" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0
[ 11.302913] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 11.325600] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 11.334274] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 11.510983] init: processing action (sys.sysctl.extra_free_kbytes=*) from (/init.rc:725)
[ 12.057749] read descriptors
[ 12.060755] read strings
[ 12.063525] read descriptors
[ 12.066436] read strings
[ 12.085743] acc_open
[ 12.087991] acc_release
[ 12.300220] Atheros 8031 ethernet 30be0000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=30be0000.ethernet-1:00, irq=POLL)
[ 12.315851] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 12.333103] type=1400 audit(1545213113.888:583): avc: denied { dac_read_search } for pid=3164 comm="Binder:3164_1" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0 duplicate messages suppressed
[ 12.352109] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 12.362840] type=1400 audit(1545213115.124:2324): avc: denied { dac_read_search } for pid=3396 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 12.422636] type=1400 audit(1545213115.128:2327): avc: denied { dac_read_search } for pid=3396 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[ 12.424148] audit: audit_lost=2263 audit_rate_limit=5 audit_backlog_limit=64
[ 12.424151] audit: rate limit exceeded
[ 12.425120] sdcardfs version 2.0
[ 12.425126] sdcardfs: dev_name -> /data/media
[ 12.425128] sdcardfs: options -> fsuid=1023,fsgid=1023,multiuser,derive_gid,default_normal,mask=6,userid=0,gid=1015
[ 12.425133] sdcardfs: mnt -> ffff80003f93f520
[ 12.425204] sdcardfs: mounted on top of /data/media type ext4
[ 12.425866] Remount options were mask=23,gid=9997 for vfsmnt ffff80003cdee560.
[ 12.425878] sdcardfs : options - debug:1
[ 12.425881] sdcardfs : options - gid:9997
[ 12.425883] sdcardfs : options - mask:23
[ 12.425988] Remount options were mask=7,gid=9997 for vfsmnt ffff80003cdeefe0.
[ 12.425994] sdcardfs : options - debug:1
[ 12.425997] sdcardfs : options - gid:9997
[ 12.425998] sdcardfs : options - mask:7
[ 12.528256] type=1400 audit(1545213115.216:2328): avc: denied { dac_read_search } for pid=3421 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 12.838706] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 13.463127] type=1400 audit(1545213115.216:2328): avc: denied { dac_read_search } for pid=3421 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 13.484373] type=1400 audit(1545213116.256:2356): avc: denied { read } for pid=3281 comm="system_server" name="state" dev="sysfs" ino=21235 scontext=u:r:system_server:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=0
[ 13.511832] type=1400 audit(1545213116.256:2356): avc: denied { read } for pid=3281 comm="system_server" name="state" dev="sysfs" ino=21235 scontext=u:r:system_server:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=0
[ 13.548648] type=1400 audit(1545213116.260:2357): avc: denied { read } for pid=3281 comm="system_server" name="state" dev="sysfs" ino=21366 scontext=u:r:system_server:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=0
[ 13.592469] audit: audit_lost=2290 audit_rate_limit=5 audit_backlog_limit=64
[ 13.592472] audit: rate limit exceeded
[ 15.478774] init: Service 'bootanim' (pid 3275) exited with status 0
[ 15.513613] init: processing action (sys.boot_completed=1) from (/init.rc:719)
[ 15.522372] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/init.freescale.imx8mm.rc:20)
[ 15.540522] audit: audit_lost=2291 audit_rate_limit=5 audit_backlog_limit=64
[ 15.548967] audit: rate limit exceeded
[ 15.561324] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/init.freescale.imx8mm.rc:27)
[ 15.581467] selinux: SELinux: Skipping restorecon_recursive(/data/system_ce/0)
[ 15.581467]
[ 15.587835] init: processing action (sys.boot_completed=1 && sys.logbootcomplete=1) from (/system/etc/init/bootstat.rc:70)
[ 15.589388] init: starting service 'exec 6 (/system/bin/bootstat --set_system_boot_reason --record_boot_complete --record_boot_reason --record_time_since_factory_reset -l)'...
[ 15.593035] init: processing action (sys.boot_completed=1 && sys.wifitracing.started=0) from (/system/etc/init/wifi-events.rc:20)
[ 15.650698] init: Command 'mkdir /sys/kernel/debug/tracing/instances/wifi 711' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi-events.rc:22) took 57ms and succeeded
[ 16.691609] type=1400 audit(1545213118.336:2366): avc: denied { dac_read_search } for pid=3065 comm="Binder:3065_3" capability=2 scontext=u:r:vold:s0 tcontext=u:r:vold:s0 tclass=capability permissive=0 duplicate messages suppressed
[ 16.712717] type=1400 audit(1545213119.484:3585): avc: denied { dac_read_search } for pid=3863 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 16.844074] type=1400 audit(1545213119.488:3588): avc: denied { dac_read_search } for pid=3863 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[ 16.872733] audit: audit_lost=3509 audit_rate_limit=5 audit_backlog_limit=64
[ 16.872738] audit: rate limit exceeded
[ 16.899687] type=1400 audit(1545213119.640:3589): avc: denied { dac_read_search } for pid=3887 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 22.679393] type=1400 audit(1545213119.640:3589): avc: denied { dac_read_search } for pid=3887 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 22.698123] type=1400 audit(1545213125.472:3605): avc: denied { dac_read_search } for pid=3980 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 22.763382] audit: audit_lost=3524 audit_rate_limit=5 audit_backlog_limit=64
[ 22.763410] type=1400 audit(1545213125.472:3608): avc: denied { dac_read_search } for pid=3980 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[ 22.763434] type=1400 audit(1545213125.556:3609): avc: denied { dac_read_search } for pid=4003 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[ 22.809034] audit: rate limit exceeded

#8MMINILPD4-EVK imx 8mm‌ android_p9.0.0_1.0.0‌ android 9.0‌ i.mx 8m evaluation kit‌ boot issue‌

0 Kudos
3 Replies

1,680 Views
mauritzbotha
Contributor III

Thanks for posting this Karl.

I have a similar issue on both of the EVKs we bought. Did not get to the trace yet. I did see a difference between the setting of the boot switches as is printed on the silk screen of the PCB and the getting started guide.

I have not been able to get mine to boot. Any suggestions would be helpful

0 Kudos

1,680 Views
don_gunn
Contributor V

I am having a similar issue.  I have rev C MX8M mini LP EVK with the SAS to HDMI adaptor connected to the DSI-MIPI connector on the board.  The preloaded Android image did not work.  I can see that Android boots on the serial console but there is nothing on the HDMI display.  I then tried loading a pre-build Android image onto the board using UUU and the scripts provided with the image.  The image loaded onto the board as expected, I then updated the u-boot environment variables as described in the documentation but there was still no image on the HDMI display.

I then tried flashing an SD card instead of the eMMC, same results.

Then I flashed the Linux image onto the SD card, configured the video in u-boot:

mmcargs=setenv bootargs ${jh_clk} console=${console} root=${mmcroot} video=${video}

video=HDMI-A-1:1920x1080@60

At this point when I boot the Linux image I get the Linux penguins on the HDMI display and then an Open Embedded splash screen while Linux is booting.  Unfortunately just before Linux finishes booting the display shuts off again.  THe display seems to shut off at the same time as the "Starting Weston Wayland Compositor (on tty7).." line appears in the console window.

I have spent a lot of time trying to get this working.  I would be very grateful for some assistance.

Here is the console during Linux boot:

U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 11:14:18 +0000)

CPU: Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 45C
Reset cause: POR
Model: FSL i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
No panel detected: default to MIPI2HDMI
Display: MIPI2HDMI (1920x1080)
Video: 1920x1080x24
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF 1cb68fa
- U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df

switch to partitions #0, OK
mmc0 is current device
flash target is MMC:0
Net: eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
** Unable to read file boot.scr **
23163392 bytes read in 995 ms (22.2 MiB/s)
Booting from mmc ...
43219 bytes read in 16 ms (2.6 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300d8d2

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea (oe-user@oe-host) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Sun Apr 14 11:10:21 UTC 2019
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: FSL i.MX8MM EVK board
[ 0.000000] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[ 0.000000] bootconsole [ec_imx6q0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000078000000, size 640 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000bdffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbdfbce00-0xbdfbebff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000bdffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 24 pages/cpu @ffff80007df57000 s57624 r8192 d32488 u98304
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507008
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 root=/dev/mmcblk1p2 rootwait rw video=HDMI-A-1:1920x1080@60
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Memory: 1348328K/2060288K available (13564K kernel code, 1692K rwdata, 6052K rodata, 1280K init, 434K bss, 56600K reserved, 655360K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008dc0000 ( 13568 KB)
[ 0.000000] .rodata : 0xffff000008dc0000 - 0xffff0000093b0000 ( 6080 KB)
[ 0.000000] .init : 0xffff0000093b0000 - 0xffff0000094f0000 ( 1280 KB)
[ 0.000000] .data : 0xffff0000094f0000 - 0xffff000009697200 ( 1693 KB)
[ 0.000000] .bss : 0xffff000009697200 - 0xffff000009703b40 ( 435 KB)
[ 0.000000] fixed : 0xffff7dfffe7f9000 - 0xffff7dfffec00000 ( 4124 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000000000 - 0xffff7e0001f80000 ( 31 MB actual)
[ 0.000000] memory : 0xffff800000000000 - 0xffff80007e000000 ( 2016 MB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] i.MX8MM clock driver init done
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000004] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.008511] system counter timer init
[ 0.011763] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.019776] clocksource: imx sysctr: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.031043] Console: colour dummy device 80x25
[ 0.034612] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.044899] pid_max: default: 32768 minimum: 301
[ 0.049594] Security Framework initialized
[ 0.054172] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.061080] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.067929] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.074656] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.097885] ASID allocator initialised with 32768 entries
[ 0.105883] Hierarchical SRCU implementation.
[ 0.114368] Cannot find MU entry in device tree
[ 0.116176] CPU identified as i.MX8MM, silicon rev 1.0
[ 0.121893] EFI services will not be available.
[ 0.133791] smp: Bringing up secondary CPUs ...
[ 0.161940] Detected VIPT I-cache on CPU1
[ 0.161966] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.161993] CPU1: Booted secondary processor [410fd034]
[ 0.189979] Detected VIPT I-cache on CPU2
[ 0.189997] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.190012] CPU2: Booted secondary processor [410fd034]
[ 0.218035] Detected VIPT I-cache on CPU3
[ 0.218051] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.218065] CPU3: Booted secondary processor [410fd034]
[ 0.218121] smp: Brought up 1 node, 4 CPUs
[ 0.267941] SMP: Total of 4 processors activated.
[ 0.272662] CPU features: detected feature: GIC system register CPU interface
[ 0.279843] CPU features: detected feature: 32-bit EL0 Support
[ 0.285699] CPU features: detected feature: Kernel page table isolation (KPTI)
[ 0.297260] CPU: All CPU(s) started at EL2
[ 0.298513] alternatives: patching kernel code
[ 0.304027] devtmpfs: initialized
[ 0.311041] random: get_random_u32 called from bucket_table_alloc+0x108/0x260 with crng_init=0
[ 0.317392] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.326682] futex hash table entries: 1024 (order: 5, 131072 bytes)
[ 0.347688] pinctrl core: initialized pinctrl subsystem
[ 0.351422] DMI not present or invalid.
[ 0.354232] NET: Registered protocol family 16
[ 0.360101] cpuidle: using governor menu
[ 0.363060] vdso: 2 pages (1 code @ ffff000008dc6000, 1 data @ ffff0000094f4000)
[ 0.369793] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.381966] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.385961] Serial: AMBA PL011 UART driver
[ 0.389676] imx rpmsg driver is registered.
[ 0.397214] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.425736] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.435608] ACPI: Interpreter disabled.
[ 0.438361] vgaarb: loaded
[ 0.439535] SCSI subsystem initialized
[ 0.444784] usbcore: registered new interface driver usbfs
[ 0.448632] usbcore: registered new interface driver hub
[ 0.454001] usbcore: registered new device driver usb
[ 0.459338] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[ 0.468005] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator
[ 0.480498] bd71837 0-004b: Device ID=0xA0
[ 0.481745] bd71837 0-004b: gpio_intr = 3
[ 0.485876] bd71837 0-004b: chip_irq=70
[ 0.497787] bd71837-pmic bd71837-pmic: regulator register name 'buck1'
[ 0.517750] bd71837-pmic bd71837-pmic: regulator register name 'buck2'
[ 0.533758] bd71837-pmic bd71837-pmic: regulator register name 'buck3'
[ 0.545804] bd71837-pmic bd71837-pmic: regulator register name 'buck4'
[ 0.557813] bd71837-pmic bd71837-pmic: regulator register name 'buck5'
[ 0.569843] bd71837-pmic bd71837-pmic: regulator register name 'buck6'
[ 0.581864] bd71837-pmic bd71837-pmic: regulator register name 'buck7'
[ 0.593895] bd71837-pmic bd71837-pmic: regulator register name 'buck8'
[ 0.605921] bd71837-pmic bd71837-pmic: regulator register name 'ldo1'
[ 0.625969] bd71837-pmic bd71837-pmic: regulator register name 'ldo2'
[ 0.633970] bd71837-pmic bd71837-pmic: regulator register name 'ldo3'
[ 0.654025] bd71837-pmic bd71837-pmic: regulator register name 'ldo4'
[ 0.674071] bd71837-pmic bd71837-pmic: regulator register name 'ldo5'
[ 0.682081] bd71837-pmic bd71837-pmic: regulator register name 'ldo6'
[ 0.702126] bd71837-pmic bd71837-pmic: regulator register name 'ldo7'
[ 0.722151] i2c i2c-0: IMX I2C adapter registered
[ 0.724011] i2c i2c-0: can't use DMA, using PIO instead.
[ 0.730049] i2c i2c-1: IMX I2C adapter registered
[ 0.734096] i2c i2c-1: can't use DMA, using PIO instead.
[ 0.739931] pca953x 2-0020: 2-0020 supply vcc not found, using dummy regulator
[ 0.778963] random: fast init done
[ 0.823784] i2c i2c-2: IMX I2C adapter registered
[ 0.825642] i2c i2c-2: can't use DMA, using PIO instead.
[ 0.832101] media: Linux media interface: v0.10
[ 0.835570] Linux video capture interface: v2.00
[ 0.840297] pps_core: LinuxPPS API ver. 1 registered
[ 0.845191] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.854363] PTP clock support registered
[ 0.858496] EDAC MC: Ver: 3.0.0
[ 0.861647] dmi: Firmware registration failed.
[ 0.866728] Advanced Linux Sound Architecture Driver Initialized.
[ 0.872492] Bluetooth: Core ver 2.22
[ 0.875624] NET: Registered protocol family 31
[ 0.880080] Bluetooth: HCI device and connection manager initialized
[ 0.886469] Bluetooth: HCI socket layer initialized
[ 0.891362] Bluetooth: L2CAP socket layer initialized
[ 0.896452] Bluetooth: SCO socket layer initialized
[ 0.902063] clocksource: Switched to clocksource arch_sys_counter
[ 0.907577] VFS: Disk quotas dquot_6.6.0
[ 0.911440] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.918425] pnp: PnP ACPI: disabled
[ 0.926991] NET: Registered protocol family 2
[ 0.928921] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.935916] TCP bind hash table entries: 16384 (order: 6, 262144 bytes)
[ 0.942641] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.949071] UDP hash table entries: 1024 (order: 3, 32768 bytes)
[ 0.955072] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
[ 0.961634] NET: Registered protocol family 1
[ 0.966275] RPC: Registered named UNIX socket transport module.
[ 0.971828] RPC: Registered udp transport module.
[ 0.976551] RPC: Registered tcp transport module.
[ 0.981274] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.988555] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.995883] kvm [1]: 8-bit VMID
[ 0.999442] kvm [1]: GICv3: no GICV resource entry
[ 1.003502] kvm [1]: disabling GICv2 emulation
[ 1.007980] kvm [1]: GIC system register CPU interface enabled
[ 1.013887] kvm [1]: vgic interrupt IRQ1
[ 1.017840] kvm [1]: Hyp mode initialized successfully
[ 1.025149] audit: initializing netlink subsys (disabled)
[ 1.028492] audit: type=2000 audit(0.888:1): state=initialized audit_enabled=0 res=1
[ 1.028784] workingset: timestamp_bits=44 max_order=19 bucket_order=0
[ 1.047773] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.051319] NFS: Registering the id_resolver key type
[ 1.055885] Key type id_resolver registered
[ 1.060056] Key type id_legacy registered
[ 1.064086] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.070836] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 1.077398] 9p: Installing v9fs 9p2000 file system support
[ 1.086719] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 1.091332] io scheduler noop registered
[ 1.095351] io scheduler cfq registered (default)
[ 1.099967] io scheduler mq-deadline registered
[ 1.104514] io scheduler kyber registered
[ 1.120989] imx-sdma 30bd0000.dma-controller: no iram assigned, using external mem
[ 1.127824] imx-sdma 30bd0000.dma-controller: Falling back to user helper
[ 1.134628] imx-sdma 302c0000.dma-controller: no iram assigned, using external mem
[ 1.144427] imx-sdma 302b0000.dma-controller: no iram assigned, using external mem
[ 1.154344] mxs-dma 33000000.dma-apbh: initialized
[ 1.158189] Bus freq driver module loaded
[ 1.166129] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.171979] SuperH (H)SCI(F) driver initialized
[ 1.175050] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 30, base_baud = 5000000) is a IMX
[ 1.183801] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 31, base_baud = 5000000) is a IMX
[ 1.192395] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 32, base_baud = 1500000) is a IMX
[ 1.203549] console [ttymxc1] enabled
[ 1.203549] console [ttymxc1] enabled
[ 1.208036] bootconsole [ec_imx6q0] disabled
[ 1.208036] bootconsole [ec_imx6q0] disabled
[ 1.217410] msm_serial: driver initialized
[ 1.228576] adv7511 1-003d: 1-003d supply avdd not found, using dummy regulator
[ 1.235948] adv7511 1-003d: 1-003d supply dvdd not found, using dummy regulator
[ 1.243320] adv7511 1-003d: 1-003d supply pvdd not found, using dummy regulator
[ 1.250664] adv7511 1-003d: 1-003d supply a2vdd not found, using dummy regulator
[ 1.258101] adv7511 1-003d: 1-003d supply v3p3 not found, using dummy regulator
[ 1.265449] adv7511 1-003d: 1-003d supply v1p2 not found, using dummy regulator
[ 1.281524] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.288167] [drm] No driver support for vblank timestamp query.
[ 1.294199] imx-drm display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 1.301869] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 1.309015] imx-drm display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[ 1.409496] Console: switching to colour frame buffer device 240x67
[ 1.447559] imx-drm display-subsystem: fb0: frame buffer device
[ 1.453876] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[ 1.467069] loop: module loaded
[ 1.474533] fsl-flexspi 30bb0000.flexspi: mt25qu256 (32768 Kbytes)
[ 1.481626] slram: not enough parameters.
[ 1.488690] libphy: Fixed MDIO Bus: probed
[ 1.493222] NXP PHY: loading NXP PHY driver: [autonomous mode]
[ 1.499239] tun: Universal TUN/TAP device driver, 1.6
[ 1.504480] CAN device driver interface
[ 1.510330] fec 30be0000.ethernet: 30be0000.ethernet supply phy not found, using dummy regulator
[ 1.519441] pps pps0: new PPS source ptp0
[ 1.528295] libphy: fec_enet_mii_bus: probed
[ 1.533392] fec 30be0000.ethernet eth0: registered PHC device 0
[ 1.540083] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.545937] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.551925] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[ 1.558900] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.564524] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.572372] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.578771] sky2: driver version 1.30
[ 1.584521] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.591086] ehci-pci: EHCI PCI platform driver
[ 1.595601] ehci-platform: EHCI generic platform driver
[ 1.601026] ehci-orion: EHCI orion driver
[ 1.605188] ehci-exynos: EHCI EXYNOS driver
[ 1.609520] ehci-msm: Qualcomm On-Chip EHCI Host Controller
[ 1.615214] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.621431] ohci-pci: OHCI PCI platform driver
[ 1.625943] ohci-platform: OHCI generic platform driver
[ 1.631347] ohci-exynos: OHCI EXYNOS driver
[ 1.636220] usbcore: registered new interface driver usb-storage
[ 1.642319] usbcore: registered new interface driver usb_ehset_test
[ 1.649669] usbmisc_imx 32e40200.usbmisc: 32e40200.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 1.659973] usbmisc_imx 32e50200.usbmisc: 32e50200.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 1.670948] imx_usb 32e40000.usb: 32e40000.usb supply vbus not found, using dummy regulator
[ 1.680882] input: 30370000.snvs:snvs-powerkey as /devices/platform/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.694008] snvs_rtc 30370000.snvs:snvs-rtc-lp: rtc core: registered 30370000.snvs:snvs-rtc-lp as rtc0
[ 1.703871] i2c /dev entries driver
[ 1.709589] IR NEC protocol handler initialized
[ 1.714156] IR RC5(x/sz) protocol handler initialized
[ 1.719220] IR RC6 protocol handler initialized
[ 1.723760] IR JVC protocol handler initialized
[ 1.728303] IR Sony protocol handler initialized
[ 1.732929] IR SANYO protocol handler initialized
[ 1.737642] IR Sharp protocol handler initialized
[ 1.742359] IR MCE Keyboard/mouse protocol handler initialized
[ 1.748202] IR XMP protocol handler initialized
[ 1.753237] Registered IR keymap rc-empty
[ 1.757335] rc rc0: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0
[ 1.764137] input: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0/input1
[ 1.771675] input: MCE IR Keyboard/Mouse (gpio-rc-recv) as /devices/virtual/input/input2
[ 1.780960] mxc_mipi-csi 32e30000.mipi_csi: 32e30000.mipi_csi supply mipi-phy not found, using dummy regulator
[ 1.791332] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered
[ 1.798310] CSI: Registered sensor subdevice: mxc_mipi-csi.0
[ 1.803999] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 333000000
[ 1.814242] ov5640_mipi 2-003c: No sensor reset pin available
[ 1.820033] ov5640_mipi 2-003c: 2-003c supply DOVDD not found, using dummy regulator
[ 1.827831] ov5640_mipi 2-003c: 2-003c supply DVDD not found, using dummy regulator
[ 1.835524] ov5640_mipi 2-003c: 2-003c supply AVDD not found, using dummy regulator
[ 1.854368] ov5640_mipi 2-003c: Read reg error: reg=300a
[ 1.859696] ov5640_mipi 2-003c: Camera is not found
[ 1.879585] imx2-wdt 30280000.wdog: timeout 60 sec (nowayout=0)
[ 1.886276] Bluetooth: HCI UART driver ver 2.3
[ 1.890741] Bluetooth: HCI UART protocol H4 registered
[ 1.895889] Bluetooth: HCI UART protocol BCSP registered
[ 1.901210] Bluetooth: HCI UART protocol ATH3K registered
[ 1.906621] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.913026] Bluetooth: HCI UART protocol Broadcom registered
[ 1.918704] Bluetooth: HCI UART protocol QCA registered
[ 1.924974] sdhci: Secure Digital Host Controller Interface driver
[ 1.931181] sdhci: Copyright(c) Pierre Ossman
[ 1.935862] Synopsys Designware Multimedia Card Interface Driver
[ 1.943072] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.949592] mmc0: CQHCI version 5.10
[ 1.998366] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 2.008083] mmc1: CQHCI version 5.10
[ 2.014142] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 2.066374] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.076208] mmc2: CQHCI version 5.10
[ 2.083331] mmc0: queuing unknown CIS tuple 0x01 (3 bytes)
[ 2.102765] mmc0: queuing unknown CIS tuple 0x1a (5 bytes)
[ 2.111678] mmc0: queuing unknown CIS tuple 0x1b (8 bytes)
[ 2.117872] mmc0: queuing unknown CIS tuple 0x14 (0 bytes)
[ 2.134088] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 2.144496] mmc0: queuing unknown CIS tuple 0x80 (1 bytes)
[ 2.149261] hantrodec 0 : module inserted. Major = 236
[ 2.150103] mmc0: queuing unknown CIS tuple 0x81 (1 bytes)
[ 2.157120] hantrodec 1 : module inserted. Major = 236
[ 2.160704] mmc0: queuing unknown CIS tuple 0x82 (1 bytes)
[ 2.166915] hx280enc: module inserted. Major <235>
[ 2.171337] mmc0: new ultra high speed SDR104 SDIO card at address 0001
[ 2.182895] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.189846] caam 30900000.caam: ERA source: CCBVID.
[ 2.198051] caam 30900000.caam: device ID = 0x0a16040100000000 (Era 9)
[ 2.204688] caam 30900000.caam: job rings = 3, qi = 0, dpaa2 = no
[ 2.221279] caam algorithms registered in /proc/crypto
[ 2.229593] caam_jr 30901000.jr0: registering rng-caam
[ 2.235002] caam 30900000.caam: caam pkc algorithms registered in /proc/crypto
[ 2.243926] platform caam_sm: blkkey_ex: 2 keystore units available
[ 2.250324] platform caam_sm: 64-bit clear key:
[ 2.254872] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 2.260509] mmc1: host does not support reading read-only switch, assuming write-enable
[ 2.260548] platform caam_sm: 64-bit black key:
[ 2.273102] platform caam_sm: [0000] 88 8d ba 3d 47 eb f2 30
[ 2.278773] platform caam_sm: [0008] f9 38 5d 8e 16 48 54 e9
[ 2.284445] platform caam_sm: 128-bit clear key:
[ 2.289074] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 2.294750] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 2.300418] platform caam_sm: 128-bit black key:
[ 2.305047] platform caam_sm: [0000] 26 97 23 9c 4c bd af 6d
[ 2.310717] platform caam_sm: [0008] ce 66 96 71 5d 50 47 03
[ 2.316064] mmc2: Command Queue Engine enabled
[ 2.316401] platform caam_sm: 192-bit clear key:
[ 2.320881] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 2.325463] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 2.332377] mmcblk2: mmc2:0001 DG4016 14.7 GiB
[ 2.337488] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 2.337495] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 2.342254] mmcblk2boot0: mmc2:0001 DG4016 partition 1 4.00 MiB
[ 2.347698] platform caam_sm: 192-bit black key:
[ 2.353581] mmcblk2boot1: mmc2:0001 DG4016 partition 2 4.00 MiB
[ 2.359291] platform caam_sm: [0000] 0e 01 76 19 40 57 d2 a1
[ 2.359298] platform caam_sm: [0008] 01 53 89 25 fc 0f b9 8a
[ 2.364128] mmcblk2rpmb: mmc2:0001 DG4016 partition 3 4.00 MiB
[ 2.369849] platform caam_sm: [0016] 4a 70 fa 97 ed b0 6c f0
[ 2.380804] Alternate GPT is invalid, using primary GPT.
[ 2.381186] platform caam_sm: [0024] 69 47 5d 2b 18 94 0e 53
[ 2.386120] mmc1: new ultra high speed DDR50 SDHC card at address aaaa
[ 2.386697] mmcblk1: mmc1:aaaa SS16G 14.8 GiB
[ 2.387064] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15
[ 2.392690] platform caam_sm: 256-bit clear key:
[ 2.408791] mmcblk1: p1 p2
[ 2.410224] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 2.410233] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 2.440164] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 2.445839] platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
[ 2.451508] platform caam_sm: 256-bit black key:
[ 2.456142] platform caam_sm: [0000] 04 63 e8 f7 b9 2b 35 0d
[ 2.461814] platform caam_sm: [0008] bf 22 3a 53 e2 ff 0e eb
[ 2.467489] platform caam_sm: [0016] cd 91 bf 64 03 8a 83 06
[ 2.473160] platform caam_sm: [0024] fb 00 f4 dc 2f 25 a2 d4
[ 2.478830] platform caam_sm: 64-bit unwritten blob:
[ 2.483810] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 2.489486] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 2.495158] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 2.500829] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 2.506501] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 2.512172] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 2.517844] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 2.523515] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 2.529186] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 2.534856] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.540527] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.546198] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.551865] platform caam_sm: 128-bit unwritten blob:
[ 2.556928] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 2.562598] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 2.568268] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 2.573938] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 2.579609] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 2.585278] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 2.590949] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 2.596620] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 2.602290] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 2.607960] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.613631] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.619300] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.624969] platform caam_sm: 196-bit unwritten blob:
[ 2.630031] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 2.635701] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 2.641372] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 2.647042] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 2.652712] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 2.658382] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 2.664053] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 2.669722] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 2.675393] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 2.681063] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.686734] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.692405] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.698073] platform caam_sm: 256-bit unwritten blob:
[ 2.703136] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 2.708806] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 2.714476] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 2.720146] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 2.725817] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 2.731487] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 2.737157] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 2.742832] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 2.748503] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 2.754173] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.759844] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.765514] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.771675] platform caam_sm: 64-bit black key in blob:
[ 2.776916] platform caam_sm: [0000] 7a f2 78 3b 60 81 24 85
[ 2.782588] platform caam_sm: [0008] 20 6f d2 26 95 80 0c 48
[ 2.788258] platform caam_sm: [0016] 1d 6b 31 6d f0 41 83 e4
[ 2.793929] platform caam_sm: [0024] ba 0e 69 9f e6 04 be 7e
[ 2.799600] platform caam_sm: [0032] 20 63 37 f3 0f c8 a2 38
[ 2.805270] platform caam_sm: [0040] 85 29 3d 8a 06 1b ed 0e
[ 2.810941] platform caam_sm: [0048] 00 fb 41 44 b3 59 00 6c
[ 2.816611] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 2.822282] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 2.827952] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.833622] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.839293] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.844961] platform caam_sm: 128-bit black key in blob:
[ 2.850285] platform caam_sm: [0000] fe 4f 8b 3c b5 26 e9 eb
[ 2.855956] platform caam_sm: [0008] ee 7f 5e 86 02 be df 63
[ 2.861627] platform caam_sm: [0016] e6 ce 6a 2d 7b 4e 48 34
[ 2.867298] platform caam_sm: [0024] 47 dd c1 0d 9e 40 52 de
[ 2.872969] platform caam_sm: [0032] 7e 6f 5f 8c 5d cf 84 97
[ 2.878640] platform caam_sm: [0040] 3b 32 f7 05 bf 99 a1 70
[ 2.884311] platform caam_sm: [0048] 9b 0a 93 fd 13 07 6c 7b
[ 2.889981] platform caam_sm: [0056] a0 24 20 ac dd 1e 3a 1f
[ 2.895652] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 2.901322] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.906993] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.912663] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.918353] platform caam_sm: 192-bit black key in blob:
[ 2.923678] platform caam_sm: [0000] d7 3f 6d c2 cb ca 3f d5
[ 2.929349] platform caam_sm: [0008] dd 39 ff c0 0d ba 94 21
[ 2.935019] platform caam_sm: [0016] 67 77 6c 12 4d 18 a0 59
[ 2.940690] platform caam_sm: [0024] b3 01 8f fe 36 98 5e 45
[ 2.946360] platform caam_sm: [0032] 15 23 a4 1f ef a5 4e 20
[ 2.952030] platform caam_sm: [0040] e1 77 20 0e 4b 39 a4 ca
[ 2.957700] platform caam_sm: [0048] 1b 88 7d c4 41 b8 04 a3
[ 2.963371] platform caam_sm: [0056] 4b ec 47 9b 26 8b 18 45
[ 2.969041] platform caam_sm: [0064] ef ee 3b 03 64 d6 6d 14
[ 2.974711] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.980382] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.986051] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.991729] platform caam_sm: 256-bit black key in blob:
[ 2.997053] platform caam_sm: [0000] 31 13 1e 40 fd 6f d3 84
[ 3.002727] platform caam_sm: [0008] 0f 19 ad b2 17 e5 5d 9e
[ 3.008398] platform caam_sm: [0016] 35 4e 5e 7b 69 80 61 2a
[ 3.014069] platform caam_sm: [0024] 60 e7 43 fc 9b d1 da 46
[ 3.019738] platform caam_sm: [0032] ed 3f fb 50 cd a9 a9 fd
[ 3.025409] platform caam_sm: [0040] ac aa 03 3a 31 d7 63 82
[ 3.031079] platform caam_sm: [0048] 6d 06 fa 63 cf c7 53 d3
[ 3.036749] platform caam_sm: [0056] 70 d0 a3 0f 28 9f 1f cc
[ 3.042419] platform caam_sm: [0064] 21 1e e5 1c c4 18 cd 8c
[ 3.048090] platform caam_sm: [0072] db 52 6f c6 dd e3 c9 13
[ 3.053760] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 3.059430] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 3.065855] platform caam_sm: restored 64-bit black key:
[ 3.071186] platform caam_sm: [0000] d6 6a c9 6a 4b 04 f8 51
[ 3.076858] platform caam_sm: [0008] d5 92 47 c0 33 df ce c3
[ 3.082527] platform caam_sm: restored 128-bit black key:
[ 3.087938] platform caam_sm: [0000] 26 97 23 9c 4c bd af 6d
[ 3.093609] platform caam_sm: [0008] ce 66 96 71 5d 50 47 03
[ 3.099277] platform caam_sm: restored 192-bit black key:
[ 3.104688] platform caam_sm: [0000] 0e 01 76 19 40 57 d2 a1
[ 3.110359] platform caam_sm: [0008] 01 53 89 25 fc 0f b9 8a
[ 3.116030] platform caam_sm: [0016] ec ab 7e fa 4b d0 15 02
[ 3.121700] platform caam_sm: [0024] a3 ea 1b 26 01 93 f9 e4
[ 3.127369] platform caam_sm: restored 256-bit black key:
[ 3.132779] platform caam_sm: [0000] 04 63 e8 f7 b9 2b 35 0d
[ 3.138451] platform caam_sm: [0008] bf 22 3a 53 e2 ff 0e eb
[ 3.144122] platform caam_sm: [0016] cd 91 bf 64 03 8a 83 06
[ 3.149792] platform caam_sm: [0024] fb 00 f4 dc 2f 25 a2 d4
[ 3.156023] caam-snvs 30370000.caam-snvs: can't get snvs clock
[ 3.161905] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state
[ 3.170479] usbcore: registered new interface driver usbhid
[ 3.176078] usbhid: USB HID core driver
[ 3.192920] optee: probing for conduit method from DT.
[ 3.198337] optee: initialized driver
[ 3.203190] ak4458 2-0010: Failed to get supply 'DVDD': -517
[ 3.208876] ak4458 2-0010: Failed to request supplies: -517
[ 3.214679] ak4458 2-0012: Failed to get supply 'DVDD': -517
[ 3.220356] ak4458 2-0012: Failed to request supplies: -517
[ 3.226189] ak4497 2-0011: Failed to get supply 'DVDD': -517
[ 3.231863] ak4497 2-0011: Failed to request supplies: -517
[ 3.239308] ak5558 2-0013: Failed to get supply 'DVDD': -517
[ 3.244987] ak5558 2-0013: Failed to request supplies: -517
[ 3.269817] fsl-micfil-dai 30080000.micfil: GET IRQ: 43
[ 3.275080] fsl-micfil-dai 30080000.micfil: GET IRQ: 44
[ 3.280332] fsl-micfil-dai 30080000.micfil: GET IRQ: 45
[ 3.285587] fsl-micfil-dai 30080000.micfil: GET IRQ: 46
[ 3.292148] imx-wm8524 sound-wm8524: wm8524-hifi <-> 30030000.sai mapping ok
[ 3.299233] imx-wm8524 sound-wm8524: ASoC: no DMI vendor name!
[ 3.308873] imx-spdif sound-spdif: snd-soc-dummy-dai <-> 30090000.spdif mapping ok
[ 3.316493] imx-spdif sound-spdif: ASoC: no DMI vendor name!
[ 3.323500] imx-micfil sound-micfil: snd-soc-dummy-dai <-> 30080000.micfil mapping ok
[ 3.331359] imx-micfil sound-micfil: ASoC: no DMI vendor name!
[ 3.345018] imx-ak4458 sound-ak4458: ASoC: CODEC DAI ak4458-aif not registered
[ 3.352263] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-517)
[ 3.360007] NET: Registered protocol family 26
[ 3.364891] NET: Registered protocol family 10
[ 3.369962] Segment Routing with IPv6
[ 3.373675] NET: Registered protocol family 17
[ 3.378138] can: controller area network core (rev 20170425 abi 9)
[ 3.384361] NET: Registered protocol family 29
[ 3.388820] can: raw protocol (rev 20170425)
[ 3.393100] can: broadcast manager protocol (rev 20170425 t)
[ 3.398777] can: netlink gateway (rev 20170425) max_hops=1
[ 3.404426] Bluetooth: RFCOMM TTY layer initialized
[ 3.409327] Bluetooth: RFCOMM socket layer initialized
[ 3.414488] Bluetooth: RFCOMM ver 1.11
[ 3.418256] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.423578] Bluetooth: BNEP filters: protocol multicast
[ 3.428819] Bluetooth: BNEP socket layer initialized
[ 3.433794] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 3.439730] Bluetooth: HIDP socket layer initialized
[ 3.444738] lib80211: common routines for IEEE802.11 drivers
[ 3.450445] 9pnet: Installing 9P2000 support
[ 3.454771] Key type dns_resolver registered
[ 3.459628] registered taskstats version 1
[ 3.486089] cpu cpu0: registered imx8mq-cpufreq
[ 3.493574] imx6q-pcie 33800000.pcie: 33800000.pcie supply epdev_on not found, using dummy regulator
[ 3.503186] OF: PCI: host bridge /pcie@0x33800000 ranges:
[ 3.508605] OF: PCI: No bus range found for /pcie@0x33800000, using [bus 00-ff]
[ 3.516101] OF: PCI: IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[ 3.522030] OF: PCI: MEM 0x18000000..0x1fefffff -> 0x18000000
[ 3.528420] imx6q-pcie 33800000.pcie: Initialize PHY with EXT REfCLK!.
[ 3.535263] imx6q-pcie 33800000.pcie: PHY Initialization End!.
[ 3.541537] imx6q-pcie 33800000.pcie: pcie phy pll is locked.
[ 3.792436] imx6q-pcie 33800000.pcie: phy link never came up
[ 3.798117] imx6q-pcie 33800000.pcie: failed to initialize host
[ 3.804043] imx6q-pcie 33800000.pcie: unable to add pcie port.
[ 3.810115] imx6q-pcie: probe of 33800000.pcie failed with error -110
[ 3.818355] imx_usb 32e40000.usb: 32e40000.usb supply vbus not found, using dummy regulator
[ 4.178546] ak4458 2-0010: ASoC: failed to probe component -6
[ 4.184381] imx-ak4458 sound-ak4458: ASoC: failed to instantiate card -6
[ 4.191232] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-6)
[ 4.198527] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:29:03 UTC (1743)
[ 4.221257] ALSA device list:
[ 4.224247] #0: wm8524-audio
[ 4.227327] #1: imx-spdif
[ 4.230129] #2: imx-audio-micfil
[ 6.140046] EXT4-fs (mmcblk1p2): recovery complete
[ 6.155256] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 6.163392] VFS: Mounted root (ext4 filesystem) on device 179:130.
[ 6.177675] devtmpfs: mounted
[ 6.181058] Freeing unused kernel memory: 1280K
[ 6.353449] systemd[1]: System time before build time, advancing clock.
[ 6.369671] systemd[1]: systemd 237 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -ID)
[ 6.391285] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 4.14-sumo (sumo)!

[ 6.422148] systemd[1]: Set hostname to <imx8mmevk>.
[ 6.524521] systemd[1]: File /lib/systemd/system/systemd-journald.service:35 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[ 6.541722] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[ 6.668766] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.675829] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 6.702206] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.710442] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 6.730207] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.737099] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 6.754495] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 6.774523] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on Journal Socket.
Mounting Kernel Debug File System...
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Listening on Network Service Netlink Socket.
Mounting Huge Pages File System...
[ OK ] Created slice system-getty.slice.
Mounting POSIX Message Queue File System...
[ OK ] Listening on Journal Socket (/dev/log).
Starting Journal Service...
Starting Create list of required st��…ce nodes for the current kernel...
[ OK ] Reached target Remote File Systems.
[ OK ] Created slice User and Session Slice.
Starting Load Kernel Modules...
[ OK ] Listening on udev Control Socket.
[ OK ] Reached target Swap.
[ 7.036066] galcore: loading out-of-tree module taints kernel.
[ OK ] Reached target Slices.
[ 7.046116] galcore: clk_get vg clock failed, disable vg!
[ 7.051899] Galcore version 6.2.4.190076
Mounting Temporary Directory (/tmp)...
[ OK ] Listening on udev Kernel Socket.
Starting udev Coldplug all Devices...
Starting Setup Virtual Console...
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Reached target Paths.
Starting Remount Root and Kernel File Systems...
[ 7.177818] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ OK ] Started Journal Service.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Started Create list of required sta��…vice nodes for the current kernel.
[ OK ] Started Load Kernel Modules.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Setup Virtual Console.
[ OK ] Started Remount Root and Kernel File Systems.
Starting Rebuild Hardware Database...
Starting Create System Users...
Starting Apply Kernel Variables...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Create System Users.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Mounted Kernel Configuration File System.
Starting Create Static Device Nodes in /dev...
[ 7.503412] systemd-journald[2123]: Received request to flush runtime journal from PID 1
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
[ OK ] Reached target Containers.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Journal Catalog...
Starting Rebuild Dynamic Linker Cache...
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Rebuild Journal Catalog.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Rebuild Hardware Database.
Starting udev Kernel Device Manager...
[ OK ] Started udev Kernel Device Manager.
Starting Network Service...
Starting Start Psplash Boot Screen...
[ OK ] Started Network Service.
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Found device /dev/ttymxc1.
[ 9.967146] imx-sdma 302b0000.dma-controller: loaded firmware 4.4
[ 9.967866] imx-sdma 30bd0000.dma-controller: loaded firmware 4.4
[ 9.968478] imx-sdma 302c0000.dma-controller: loaded firmware 4.4
[ 9.974452] qca9377: loading driver v4.5.23.1
[ 9.992797] hifDeviceInserted: Dumping clocks (50000000,400000000)
[ 9.999151] AR6000: Set async interrupt delay clock as 2.
[ 10.144345] AR6000: configuration opcode 3 is not used for Linux SDIO stack
[ 10.155246] NUM_DEV=1 FWMODE=0x2 FWSUBMODE=0x0 FWBR_BUF 0
[ 10.406604] EXT4-fs (mmcblk2p10): warning: mounting unchecked fs, running e2fsck is recommended
[ 10.421713] EXT4-fs (mmcblk2p10): mounted filesystem without journal. Opts: (null)
[ 10.463916] EXT4-fs warning (device mmcblk2p12): ext4_enable_quotas:5685: Failed to enable quota tracking (type=-1, err=-3). Please run e2fsck to fix.
[ 10.478013] EXT4-fs (mmcblk2p12): mount failed
[ 10.484926] EXT4-fs (mmcblk2p5): warning: mounting unchecked fs, running e2fsck is recommended
[ 10.494362] EXT4-fs (mmcblk2p5): mounted filesystem without journal. Opts: (null)
[ 10.603680] random: crng init done
[ 10.607093] random: 7 urandom warning(s) missed due to ratelimiting
[ 10.640927] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Started Rebuild Dynamic Linker Cache.
Starting Update is Completed...
[ 10.721784] HIF Interrupt processing is SYNC ONLY
[ 10.726568] AR6000: configuration opcode 7 is only used for RTOS systems, not Linux systems
[ 10.734972] AR6000: configuration opcode 5 is not used for Linux SDIO stack
[ OK [ 10.742760] +HWT
] Started Update is Completed.
[ 10.750343] -HWT
[ 10.752244] MAILBOX SWAP Service is enabled!
[ 10.756549] Reduced Tx Complete service is enabled!
[ 10.762722] HTCConnectService, host indicate support b2b bundle
[ 10.769840] HTCConnectService, firmware decide to disabled b2b bundle
[ 10.776950] HTCConnectService, host indicate support b2b bundle
[ 10.783456] HTCConnectService, firmware decide to disabled b2b bundle
[ OK ] Reached target System Initialization.
[ 10.803864] ar6k_wlan mmc0:0001:1: Falling back to user helper
[ 10.811810] target uses HTT version 3.51; host uses 3.28
Starting Console System Startup Logging...
[ 10.824184] Host SW:4.5.23.1, FW:0.0.0.27, HW:QCA93x7_REV1_1
[ 10.831445] ol_pktlog_init: pktlogmod_init successfull
[ 10.836773] ath_hif_sdio: HIF (Atheros/multi-bss)
[ 10.841668] qca9377: driver loaded in 864000
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
[ OK ] Listening on dropbear.socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Periodic Command Scheduler.
Starting Login Service...
[ OK ] Started Updates psplash to basic.
[ OK ] Started TEE Supplicant.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Login Service.
Starting Connection service...
Starting Save/Restore Sound Card State...
Starting Telephony service...
[ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S).
Starting RPC Bind Service...
[ OK ] Started Job spooling tools.
Starting Network Time Service (one-shot ntpdate mode)...
Starting System Logging Service...
[ OK ] Started Console System Startup Logging.
[ OK ] Started Save/Restore Sound Card State.
[ OK ] Started RPC Bind Service.
[ OK ] Started Network Time Service (one-shot ntpdate mode).
[ OK ] Started System Logging Service.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Telephony service.
[ OK ] Started Connection service.
Starting Hostname Service...
Starting WPA supplicant...
Starting Kernel Logging [ 11.450915] Atheros 8031 ethernet 30be0000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=30be0000.ethernet-1:00, irq=POLL)
Service...
[ 11.466798] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ OK ] Reached target Sound Card.
[ OK ] Started WPA supplicant.
[ OK ] Reached target Network.
Starting Permit User Sessions...
Starting /etc/rc.local Compatibility...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started Update psplash to network.
Starting Terminate Psplash Boot Screen...
[ OK ] Started Permit User Sessions.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Started Terminate Psplash Boot Screen.
[ OK ] Started Hostname Service.
[ OK ] Started Serial Getty on ttymxc1.
[ OK ] Started Getty on tty1.
[ OK ] Reached target Login Prompts.
Starting Weston Wayland Compositor (on tty7)...
[ OK ] Started Kernel Logging Service.
[ OK ] Started Weston Wayland Compositor (on tty7).
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
[ 12.013996] audit: type=1006 audit(1550694265.656:2): pid=3919 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1

NXP i.MX Release Distro 4.14-sumo imx8mmevk ttymxc1

imx8mmevk login:

0 Kudos

1,680 Views
diegoadrian
NXP Employee
NXP Employee

I apologize for the delay.

Can you please share the steps of how you downloaded the Android image into your boar?

This is because I do not have any problem booting the Android image in the i.MX8Mmini.

Best regards,

Diego. 

0 Kudos