IMX8MM board bring up USB and Console issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM board bring up USB and Console issue

1,265 Views
divyeshmarne0
Contributor III

Hi Team,

We are doing bring up of imx8mm board.

Initially emmc chip is blank.

And we are planning to flash UUU build using usb and console.

UUU build has emmc 8gb, sdcard, console uart 4, usb2.0, pim, ddr4 changes.

But when we try to load this uuu pkg in Imx8mm chip in download mode, usb is not detecting and console is giving random garbage values at boadrate 115200.

Whenever we put device in download mode usb is not detecting to flash uuu build.

 

Please share your inputs here asap. Its very urgent.

 

Thanks

 

Labels (1)
0 Kudos
6 Replies

1,238 Views
divyeshmarne0
Contributor III

hi,

BSP version: 5.11

0 Kudos

1,244 Views
divyeshmarne0
Contributor III

Hi USB and Console is working.

We have tested DDR4 with latest RPA version on mscale tool.

And successfully integrated ddr_timing.c file in code base.

But when we are trying to flash. We are able to load only sbl code not an entire uuu build.

We are using DDR4 with PCA​ pmic . But not able to isolate BD pmic from code in uboot side.

Could you please suggest what are the changes required to integrate ddr4 with pca pmic.

​Will provide more logs with progress on the same nxp case.

U-Boot SPL 2021.04-00002-gd9acfe2-dirty (Apr 11 2022 - 18:50:37 +0530)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 2400MTS
Training FAILED

0 Kudos

1,231 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the BSP released in our website:https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

For the newer BSP support the PCA PMIC default.

0 Kudos

1,222 Views
divyeshmarne0
Contributor III

Yes.

We are using Imx8mm custom board with Android 11 code base.

We have made following changes in code base:

1. Changes LPDDR4 to DDR4

2. Type-C to USB2.0 Micro

3. Emmc 8GB configuration

We are able to configure DDR4 with PMIC changes. u-boot is booting properly but kernel is getting stucked.

 

Thanks

0 Kudos

1,242 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using

0 Kudos

1,247 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using and how about the boot up mode?

0 Kudos