IMX8MM | How to generate a custom wake up words in VoiceSpot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MM | How to generate a custom wake up words in VoiceSpot

861 次查看
shai_b
Senior Contributor II

Dear team,

My customer is using iMX8MMINI and they plan to use VoiceSpot to wake up our MPU.

Can you please advise how the customer add a custom model to VoiceSpot to wake up his MPU?

In NXP GitHub there is ONLY a Bin file for the "Hey NXP" voiceSpot model and the customer needs to make and test VoiceSpot models for other wake words such as "Amazon".

Waiting for your kind feedback, many thanks.

Shai

VoiceSpot FAQ 

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

768 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @shai_b

For more information about this technology please contact with the VoiceSpot special team at Voice@nxp.com

Also, you can see this link: VoiceSpot Wake Word Engine | NXP Semiconductors

Have a great day!

0 项奖励
回复

768 次查看
anthonyrose
Contributor I

i have the same problem.

the FAQ says it's possible but not more than that. I'm building my prototype with porcupine.  i trained my model very fast without any dataset and it was very easy. I don't understand why NXP needs a dataset.

Q: Are custom wake words supported? 

A: Yes, custom wake words can be created as per customer request. A dataset is needed to create a custom wake word, which can either be provided by the customer or collected by NXP at additional cost. 

0 项奖励
回复