IMX8MM EVK: Purpose of using FET in DCDC (5V) MP8759GD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM EVK: Purpose of using FET in DCDC (5V) MP8759GD

Jump to solution
1,139 Views
haryanl
Contributor IV

Hi Everyone!


In the reference Schematic of IMX8M Mini, can anyone show me the purpose of using FET Q903 (NX3008NBKW, 115)?

How does it affect the Enable of DCDC MP8759?

In the datasheet of NX3008NBKW, VGS (th) = 0.6 0.9 1.1V (~ Min Type Max)
By default VBUS_IN = 5V, Q903, VGS = 0.36V (<VGSth) means that Q903 will be off. So, what function does Q903 have?
And, in case I want to use VBUS_IN = 12V, how does it affect the Enable of DCDC MP8759?

pastedImage_1.png

(Page 12 of Schematic)

Best Regards,

Yah

0 Kudos
1 Solution
1,032 Views
haryanl
Contributor IV

I'm sorry

I have understood the principle of operation

MP8759 Datasheet(Page14):

[set the EN voltage above the EN rising threshold(1.35V) and below the 4.5V absolute maximum rating.
The rising threshold should be set to provide enough hysteresis to allow for any input supply variations.]

So it is necessary to use FET

View solution in original post

0 Kudos
1 Reply
1,033 Views
haryanl
Contributor IV

I'm sorry

I have understood the principle of operation

MP8759 Datasheet(Page14):

[set the EN voltage above the EN rising threshold(1.35V) and below the 4.5V absolute maximum rating.
The rising threshold should be set to provide enough hysteresis to allow for any input supply variations.]

So it is necessary to use FET

0 Kudos