IMX8M Plus boot and read from SD Card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8M Plus boot and read from SD Card

跳至解决方案
2,512 次查看
www1519
Contributor III

Hi! NXP Engineer

This project is designed to use the IMX8M Plus platform, and include the circuit for SD Card.

In my design, the Load Switch of the PCA9450C is not used for the power supply of the SD Card,

and one DC-DC 3.3V power supply (the reason is relatively far away) is used.

However, When the PCB board is debugded, found that if the load Switch circuit of the PCA9450C

is not used, the IMX8M Plus cannot boot from the SD Card and cannot read the SD Card,

and the  driver for SD Card is also placed in the kernel, and then difficult to design change.

However, neither the manual for the IMX8M Plus nor the PCA9450C, 

the Load Switch must not be used for SD Card. Can you tell me what caused it,

and why the Load Switch function must be used?

Best regard. Thank you!

 

0 项奖励
回复
1 解答
2,309 次查看
www1519
Contributor III

Hi! joanxie @joanxie 

I'm very sorry for the late reply.

If use the Load Switch Power, can boot from SD Card.

Thank you for support.

Best regard!

 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,477 次查看
joanxie
NXP TechSupport
NXP TechSupport

how did you connect the pins if you don't use SW? pls share the schematic, I suggest that you can use this when you use PCA9450

0 项奖励
回复
2,475 次查看
www1519
Contributor III

Hi! Mr. joanxie @joanxie 

The schematic is below. In my design, SD Card‘s PS is from DCDC3.3V.

R0935,R2133,R2137 is DNP in my design.

Why  the LD must be used ?  Pls tell me, Thanks a lot.

 

www1519_3-1682332844306.png

 

www1519_2-1682332795377.png

www1519_4-1682332923871.png

www1519_5-1682333049844.png

 

 

 

 

 

0 项奖励
回复
2,465 次查看
joanxie
NXP TechSupport
NXP TechSupport

I don't they you must use it, switch loader has overcurrent protection and short circuit protection, so we suggest that customer can use it, refer to the data sheet, if you don't use SWIN and SWout, Leave it floating if not used, and as you said you couldn't boot up from sd card when you didn't use it, what message did you get?

0 项奖励
回复
2,443 次查看
www1519
Contributor III

Hi! Mr. joanxie @joanxie 

Thanks for your reply.

The log is as the following.Pls reference.

best regards.

SD启动失败log.png

emmc启动后SD错误log.png

  

0 项奖励
回复
2,429 次查看
joanxie
NXP TechSupport
NXP TechSupport

what do these pics stand for? the pic1 shows the board couldn't boot, but pic2 shows the board boot up successfully? could you share the whole logfile? if you don't use switch load, did you leave float SWIN and SWOUT?

0 项奖励
回复
2,310 次查看
www1519
Contributor III

Hi! joanxie @joanxie 

I'm very sorry for the late reply.

If use the Load Switch Power, can boot from SD Card.

Thank you for support.

Best regard!

 

0 项奖励
回复