IMX8M PLUS : GPU crash on android-10.0.0_2.6.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M PLUS : GPU crash on android-10.0.0_2.6.0

4,869 Views
mps
Contributor I

We are seeing seeing GPU crash for any GPU related operations.

On the logcat I am seeing below errors, followed by GPU crash. Please see attached GPU_crash_app.txt and GPU_crash_youtube.txt

02-12 00:27:20.401  1625  1649 W OpenGLRenderer: dequeueBuffer failed, error = -110; switching to fallback
02-12 00:27:24.405  1625  1649 W OpenGLRenderer: dequeueBuffer failed, error = -110; switching to fallback
02-12 00:27:28.406  1625  1649 W OpenGLRenderer: dequeueBuffer failed, error = -110; switching to fallback
02-12 00:27:28.408  1625  1649 I OpenGLRenderer: Davey! duration=12010ms; Flags=0, IntendedVsync=49150539834, Vsync=49150539834, OldestInputEvent=9223372036854775807, NewestInputEvent=0, HandleInputStart=49150769625, AnimationStart=49150788625, PerformTraversalsStart=49150790375, DrawStart=49151046125, SyncQueued=49151294500, SyncStart=49151493250, IssueDrawCommandsStart=49151594250, SwapBuffers=49153421125, FrameCompleted=61161710500, DequeueBufferDuration=0, QueueBufferDuration=407000,
02-12 00:27:28.409  1625  1649 W OpenGLRenderer: reserveNext failed, error = -2147483648 (Unknown error -2147483648)
02-12 00:27:49.041   670  1008 W OpenGLRenderer: dequeueBuffer failed, error = -110; switching to fallback
02-12 00:27:53.051   670  1008 W OpenGLRenderer: dequeueBuffer failed, error = -110; switching to fallback

 

cheers,

mohit

 

0 Kudos
Reply
4 Replies

4,852 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

Please accept my apologies, but this device is not currently supported since it is still in pre-production. Thank you for your comprehension!

 

BR,

Ivan.

0 Kudos
Reply

4,844 Views
mps
Contributor I

Hi @IvanRuiz ,

   As per release notes, it is supported. Pasting below the relevant section :

"1 Release Description
i.MX android-10.0.0_2.6.0 is a GA (RFP) release for Android 10 on NXP's i.MX
8M Mini, i.MX 8M Nano, i.MX 8M Plus, i.MX 8M Quad, i.MX 8QuadMax, i.MX
8QuadXPlus, and i.MX 7ULP applications processors."

 

cheers,

mohit

0 Kudos
Reply

4,822 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

As I mentioned before, the device is still in pre-production as you can see in the following link to date of this reply: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

It will be supported as soon as it is released. Thank you for your comprehension!

 

BR,

Ivan.

0 Kudos
Reply

4,812 Views
mps
Contributor I

Hi @IvanRuiz ,

  We have previously release Android 10.0.0_2.5.0 on this(A1) silicon w/o this issue.

So are you implying that Android Release Notes for Rev. android-10.0.0_2.6.0 — 15 January 2021 is incorrect?

 

cheers,

mohit

0 Kudos
Reply