Hi, I am trying to flash custom build images from i.MX_Yocto_Project_User_Guide document. I could not flash with custom uboot image and rfs. What could be the issue?
I am getting below error,
D:\images>uuu.exe -b emmc_all images_123023032021\imx-boot-imx8mnevk-sd.bin-flash_evk images_123023032021\core-image-minimal-imx8mnevk-20210323021218.rootfs.wic.bz2
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.72-0-g8e9e189
Success 0 Failure 1
1:3 1/ 1 [HID(W):LIBUSB_ERROR_TIMEOUT ] SDPS: boot -f images_123023032021\imx-boot-imx8mnevk-sd.bin-flash_evk
解決済! 解決策の投稿を見る。
Hi,
Even with the default ddr4_timing.c file I could boot successfully with device tree changes as below in kernel and build imx8mnevk.conf file.
Changes are as below in kernel source code for my samsung DDR4 of 512MB model K4A4G165WF-BCTD,
diff --git a/arch/arm64/boot/dts/freescale/imx8mn.dtsi b/arch/arm64/boot/dts/freescale/imx8mn.dtsi
index 5d4c245376b0..2b619745f67e 100644
--- a/arch/arm64/boot/dts/freescale/imx8mn.dtsi
+++ b/arch/arm64/boot/dts/freescale/imx8mn.dtsi
@@ -151,7 +151,7 @@
memory@40000000 {
device_type = "memory";
- reg = <0x0 0x40000000 0 0x80000000>;
+ reg = <0x0 0x40000000 0 0x60000000>;
};
resmem: reserved-memory {
@@ -163,8 +163,8 @@
linux,cma {
compatible = "shared-dma-pool";
reusable;
- size = <0 0x28000000>;
- alloc-ranges = <0 0x40000000 0 0x60000000>;
+ size = <0 0xa000000>;
+ alloc-ranges = <0 0x40000000 0 0x50000000>;
linux,cma-default;
};
};
In imx-yocto-bsp/sources/meta-imx/meta-bsp/conf/machine/imx8mnevk.conf
I modified as below,
- required conf/machine/imx8mnlpddr4evk.conf
+ required conf/machine/imx8mnlpddr4evk.conf
And I configured with bitbake -c menuconfig virtual/kernel
Library routines->DMA Contiguous Memory Allocator->Size in Mega Bytes
I have kept 160MB for my 512MB ram. One can increase or decrease according to there RAM size.
After all these, I could compile and build and boot successfully.
Thank you Zhiming and NXP for the support.
Hi
It is usb issue, your pc cannot communicate with evk.Please check the download mode on board.
BR
Zhiming
Hi Zhiming,
But I could flash the default uboot and custom rfs image successfully.
Issue should be something else.
Thank you,
Sandeep Raj
Can you provide the steps you build image?
Hi,
I have used below command to generate the image,
$mkdir imx-yocto-bsp
$cd imx-yocto-bsp
$repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.1.xml
$repo sync
$cd /home/sandeepraj/imx-yocto-bsp
$DISTRO=fsl-imx-wayland MACHINE=imx8mnevk source imx-setup-release.sh -b build-wayland
$pwd
/home/sandeepraj/imx-yocto-bsp/build-wayland
$bitbake -k core-image-minimal
Hi
I haven't found any release message about L5.4.70_2.3.1 in official site
It haven't been released.You can try 2.3.0
BR
Zhiming
Hi,
Even with the default ddr4_timing.c file I could boot successfully with device tree changes as below in kernel and build imx8mnevk.conf file.
Changes are as below in kernel source code for my samsung DDR4 of 512MB model K4A4G165WF-BCTD,
diff --git a/arch/arm64/boot/dts/freescale/imx8mn.dtsi b/arch/arm64/boot/dts/freescale/imx8mn.dtsi
index 5d4c245376b0..2b619745f67e 100644
--- a/arch/arm64/boot/dts/freescale/imx8mn.dtsi
+++ b/arch/arm64/boot/dts/freescale/imx8mn.dtsi
@@ -151,7 +151,7 @@
memory@40000000 {
device_type = "memory";
- reg = <0x0 0x40000000 0 0x80000000>;
+ reg = <0x0 0x40000000 0 0x60000000>;
};
resmem: reserved-memory {
@@ -163,8 +163,8 @@
linux,cma {
compatible = "shared-dma-pool";
reusable;
- size = <0 0x28000000>;
- alloc-ranges = <0 0x40000000 0 0x60000000>;
+ size = <0 0xa000000>;
+ alloc-ranges = <0 0x40000000 0 0x50000000>;
linux,cma-default;
};
};
In imx-yocto-bsp/sources/meta-imx/meta-bsp/conf/machine/imx8mnevk.conf
I modified as below,
- required conf/machine/imx8mnlpddr4evk.conf
+ required conf/machine/imx8mnlpddr4evk.conf
And I configured with bitbake -c menuconfig virtual/kernel
Library routines->DMA Contiguous Memory Allocator->Size in Mega Bytes
I have kept 160MB for my 512MB ram. One can increase or decrease according to there RAM size.
After all these, I could compile and build and boot successfully.
Thank you Zhiming and NXP for the support.
Hi,
I could see the latest release 5.4.70-2.3.1 at below link,
README - imx-manifest - i.MX Release Manifest (codeaurora.org)
Is this link not correct or latest release has issues?
Thank you