I use the android-10.0.0_2.6.0 Demo Image on iMX8MMEVK
But it can't boot up to the android desktop,
It will always see the following log to loop.
[ 166.085447] init: starting service 'vendor.thermal-hal-2-0'...
[ 166.239866] init: Service 'vendor.thermal-hal-2-0' (pid 606) received signal 6
[ 166.247287] init: Sending signal 9 to service 'vendor.thermal-hal-2-0' (pid 606) process group...
[ 166.256702] libprocessgroup: Successfully killed process cgroup uid 1000 pid 606 in 0ms
[ 166.265140] init: updatable process 'vendor.thermal-hal-2-0' exited 4 times before boot completed
[ 166.275326] init: Init cannot set 'ro.init.updatable_crashing_process_name' to 'vendor.thermal-hal-2-0': Read-only property was already set
[ 166.288079] init: Init cannot set 'ro.init.updatable_crashing' to '1': Read-only property was already set
[ 166.298208] init: Untracked pid 611 exited with status 0
[ 166.303779] init: Untracked pid 609 exited with status 0
And the screen keeps showing "android"
Thanks in Advance.
Regards,
Hi,
I have the same issue on imx8mp after I disabled CONFIG_BATTERY_DUMMY in kernel.
My solution I remark Thermal HAL in "./device/nxp/*/*/*.mk".
#PRODUCT_PACKAGES += \
# android.hardware.thermal@2.0-service.imx
Hi,
I am facing the same issue. Hangs in android boot logo and in logs vendor.thermal-hal service is getting restarted.
Did you get any solution to resolve the vendor.thermal-hal issue.
Regards,
Bansidaran