IMX8M MINI INTEGRATION WITH CUSTOM LVDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M MINI INTEGRATION WITH CUSTOM LVDS

3,545 Views
VinithNama
Contributor III
Hi sir,
                   we are working on panasys 10.04-inch display by using sn65dsi83 as bridge converter.
1.We have added DSI Tuner values in the sn65dsi83_brg.c file and kept some kernel messages.
2.We have updated dts file with the display parameters.
3.We can be able to read the i2c register details.
4.We added the panel-sn65dsix.c file in the gpu/drm/panel directory.
 
I'm sharing you the logs and the source files that we are working, can you share the feedback about where we are doing mistake.
0 Kudos
Reply
1 Reply

3,528 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinith

 

unfortunately nxp has not reference board with sn65dsi83 chip, so not possible to verify those patches.

Please accept our apologies.

 

Best regards
igor

0 Kudos
Reply