IMX8M LPDDR4 choice and hw design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M LPDDR4 choice and hw design

Jump to solution
1,609 Views
brsmnc
Contributor II

Hi all,

I have IMX8MQ EVKB board which uses 3GB MT53E768M32D4 LPDDR4 ram and another IMX8MM EVK board which uses 2GB (MT53D512M32D2) LPDDR4 ram.

I found these rams are pin, clock and power compatible so I think I can use 2GB MT53D512M32D2 for my all IMX8MQ and IMX8MM boards. But, when I check the reference schematics I found that IMX8MM EVK board have reversed A/B channels. CPU's A channel is connected to RAM's B channel and CPU's B channel is connected to RAM's A channel. Plese check the reference schematics below. I think this is done because of making routing easy. A and B channels works symmetrically. Am I right?

If so, I can route all my IMX8MM and IMX8MQ CPUs and MT53D512M32D2 RAMs and may be MT53E768M32D4 RAMs straight. A<->A, B<->B. Could you correct me?

IMX8MM EVK, MT53D512M32D2IMX8MM EVK, MT53D512M32D2IMX8MQ EVKB, MT53E768M32D4IMX8MQ EVKB, MT53E768M32D4

0 Kudos
1 Solution
1,598 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Yes you're correct Channel A/B were swapped on i.MX8MM EVK for easier signal routing.

There should be no problem swapping back A/B in your design. Also, it may be useful for you to take a look to the HDG for the i.MX 8M & 8MM for reference.

i.MX 8MDQLQ Hardware Developer’s Guide

i.MX 8M Mini Hardware Developer’s Guide

Regards,
Aldo.

View solution in original post

2 Replies
1,589 Views
brsmnc
Contributor II

Yes, I already have these docs. Thank you for reply

0 Kudos
1,599 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Yes you're correct Channel A/B were swapped on i.MX8MM EVK for easier signal routing.

There should be no problem swapping back A/B in your design. Also, it may be useful for you to take a look to the HDG for the i.MX 8M & 8MM for reference.

i.MX 8MDQLQ Hardware Developer’s Guide

i.MX 8M Mini Hardware Developer’s Guide

Regards,
Aldo.