IMX8M-EVK: Failed to boot from SDCARD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M-EVK: Failed to boot from SDCARD

508 Views
kamkam
Contributor I

Hi NXP,

I'm working on IMX8M-EVK

At first, I've created the imx-multimedia-image successfuly. Booting from SDCARD.

Today, I've launched bitbake again to create the imx-image-full.

Build succeeded, but it failed to boot !

 

I  have the following error message:

 

EFI boot manager: Cannot load any image

switch to partitions #0, OK

mmc0(part 0) is current device

** Unrecognized filesystem type **

Running BSP bootcmd ...

switch to partitions #0, OK

mmc1 is current device

Failed to load 'boot.scr'

Invalid FAT entry

** Unable to read file Image **

Failed to load 'Image'

Booting from net ...

BOOTP broadcast 1

 

I have regenerated the dtb files...But it still fails.

 

Any idea ?

 

 

Tags (2)
0 Kudos
Reply
1 Reply

499 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello Kam,

  • Please let me know what processes you flash the image that you build, 
  • May you have a try to flash pre-built images for the same? let's see how it is going.
  • With check the error message, which seems got stuck with kernel.

 

Best regards

Harvey

0 Kudos
Reply