IMX8M 支持SSD固态硬盘容量

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M 支持SSD固态硬盘容量

2,530件の閲覧回数
小辉哥
Contributor III

你好各位版主,关于IMX8M系列的产品,最大支持的SSD固态硬盘的容量是多少呢,是否支持2TBusb 接口的?usb 接口的和pci接口,SATA接口的应该是一样的吧,还是有区别的?我们是在linux系统下使用。期待你们的回复,谢谢!

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,420件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi,

Please see my response for your below query:

Query: "Hello, moderators, regarding the IMX8M series products, what is the maximum supported SSD solid state drive capacity, does it support 2TBusb interface? USB interface and PCI interface, SATA interface should be the same, or is there a difference? We are using it under the linux system. Looking forward to your reply, thank you!"

Ans: i.MX8M series doesn't have the direct support of SATA interface

Mrudang

0 件の賞賛
返信

2,420件の閲覧回数
小辉哥
Contributor III

谢谢你了,我知道了

0 件の賞賛
返信