IMX8DX core A35 power supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8DX core A35 power supply

1,035 Views
ceng_guanghui
Contributor II

Hello

        About IMX8DX core A35 power supply.See the datesheet as below

 Overdrive mode,the typ voltage is1.1V

 Nominal mode,the tye voltage is 1.0V

In the hardware design to choose one ,what's your suggestion

Thanks.

Zeng

0 Kudos
Reply
2 Replies

912 Views
neusch
Contributor II

What effect does the mode have for the lifetime ?
The effect at MX6 is impressive: Consumer 1,2GHz / Industrial 800MHz

Is ther any information about MX8 (overdrive/normal mode) ?

0 Kudos
Reply

971 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Depending on applications customer can use Overdrive or Nominal mode for VDD_A35 (Power

supply of Cortex-A35 cluster). For applications, where performance is the main requirement, the

Overdrive mode can be applied; for power saving - Nominal mode may be recommended.   

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.