Hello
About IMX8DX core A35 power supply.See the datesheet as below
Overdrive mode,the typ voltage is1.1V
Nominal mode,the tye voltage is 1.0V
In the hardware design to choose one ,what's your suggestion
Thanks.
Zeng
Hello,
Depending on applications customer can use Overdrive or Nominal mode for VDD_A35 (Power
supply of Cortex-A35 cluster). For applications, where performance is the main requirement, the
Overdrive mode can be applied; for power saving - Nominal mode may be recommended.
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.