IMX8DX UUU boot failed use usb-OTG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8DX UUU boot failed use usb-OTG

861 Views
ASCE00
Contributor II

Hi,all

  i'm using uuu to boot my customed IMX8DX board,had a problem like this:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.43-0-ga9c099a

Success 0 Failure 0


1:2 1/ 1 [=================100%=================] SDPS: boot -f imx-boot-imx8dxmek-sd.bin-flash

 it just stoped here and reset automatically. the board is directlly connected to PC,also the power and osclator frequency is correct.

Do you had problem like this? or have any sugggestions?

Thank you very much.

Tags (1)
0 Kudos
Reply
1 Reply

857 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using? Have you finishing poring the BSP to this board? And have you used the proper images for this board?

0 Kudos
Reply