IMX8 imx-image-full qt5 pkg connection issue with VPN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8 imx-image-full qt5 pkg connection issue with VPN

跳至解决方案
1,879 次查看
lchen
Contributor III

Hi,

I have successfully build imx-image-multimedia image for imx8qmmek. When I built imx-image-full image or SDK, the qt related pkgs always stuck at do_fetch job if my building machine is connected to company VPN. If I disconnect VPN and just use home network, the qt pkgs fetching works fine.

Is it because company firewall is blocking qt5 source? I can access the qt5 github from the browser.

Thanks,

Lijun

0 项奖励
回复
1 解答
1,865 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复
2 回复数
1,874 次查看
lchen
Contributor III

Never mind, I retried and passed this time.

0 项奖励
回复
1,866 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

(y)

 

0 项奖励
回复